在“线程: DLPC3436”中讨论的其他部件
我们刚刚开始使用DLPDLCR230NPEVM,并通过运行python脚本开始工作。 sample02_splash.py工作起来非常出色-所有的色彩都是鲜艳明亮的。 但是,一旦我们尝试显示Raspberry PI桌面或来自RPI的.mp4,图像将全部显示为绿色。 当直接从RPI显示时,似乎只有绿色LED才会激活。 原因可能是什么?
正如我所提到的,所有LED都已激活,用于"闪屏"示例。 但是,对于其他几个python示例脚本,红色和蓝色LED未激活。 例如,当显示“白色”时,“sample01_TPG.py”将显示全绿色屏幕。 大多数显示测试仅显示绿色,或者在要显示红色或蓝色时显示黑色。 值得注意的是,"执行器"测试似乎显示正确,每个像素内显示所有颜色(RGB)。 另外值得注意的是,运行sample03_display.py时,"循环图像幕帘设置"的所有测试颜色都正确。 RGB,青色,品红色等全部填充屏幕。 最后,运行sample05_led.py时,红色和蓝色测试确实有可见光,只是没有像绿色测试那样充满屏幕的任何部分,可见的内容令人难以置信地暗。
我们确实打算使用Raspberry Pi Zero W 2代替4B+,但是我们已经使用Zero和4B+进行了测试,绿色LED问题仍然完全相同(我们只需更换microSD卡)。 RPI Zero W 2通过焊接包容式管座连接,4B+通过EVM提供的管座连接器连接。
所有颜色的闪屏显示示例:
![](https://e2e.ti.com/resized-image/__size/320x240/__key/communityserver-discussions-components-files/94/PXL_5F00_20220327_5F00_001209314.jpg)
![](https://e2e.ti.com/resized-image/__size/320x240/__key/communityserver-discussions-components-files/94/PXL_5F00_20220327_5F00_001000712.MP.jpg)
示例01 -"显示:实线野白色":
![](https://e2e.ti.com/resized-image/__size/320x240/__key/communityserver-discussions-components-files/94/PXL_5F00_20220327_5F00_001532843.jpg)
"执行器测试模式"
![](https://e2e.ti.com/resized-image/__size/320x240/__key/communityserver-discussions-components-files/94/PXL_5F00_20220327_5F00_001931452.jpg)
config.txt:
# For more options and information see # http://rpf.io/configtxt # Some settings may impact device functionality. See link above for details # ######################################### # DO NOT MODIFY THE LINES BELOW THIS POINT # ######################################### # uncomment if you get no picture on HDMI for a default "safe" mode #hdmi_safe=1 # uncomment this if your display has a black border of unused pixels visible # and your display can output without overscan disable_overscan=1 # uncomment the following to adjust overscan. Use positive numbers if console # goes off screen, and negative if there is too much border #overscan_left=16 #overscan_right=16 #overscan_top=16 #overscan_bottom=16 # uncomment to force a console size. By default it will be display's size minus # overscan. #framebuffer_width=1280 #framebuffer_height=720 # uncomment if hdmi display is not detected and composite is being output hdmi_force_hotplug=1 # uncomment to force a specific HDMI mode (this will force VGA) hdmi_group=2 hdmi_mode=82 # uncomment to force a HDMI mode rather than DVI. This can make audio work in # DMT (computer monitor) modes #hdmi_drive=2 # uncomment to increase signal to HDMI, if you have interference, blanking, or # no display config_hdmi_boost=4 # uncomment for composite PAL #sdtv_mode=2 #uncomment to overclock the arm. 700 MHz is the default. #arm_freq=800 # Additional overlays and parameters are documented /boot/overlays/README # Enable audio (loads snd_bcm2835) dtparam=audio=on # Uncomment this to enable infrared communication. #dtoverlay=gpio-ir,gpio_pin=17 #dtoverlay=gpio-ir-tx,gpio_pin=18 # ######################################### # DO NOT MODIFY THE LINES ABOVE THIS POINT # ######################################### # Uncomment some or all of these to enable the optional hardware interfaces #dtparam=i2c_arm=on #dtparam=i2s=on dtparam=spi=on # Configure Raspberry PI for SSH over USB dtoverlay=dwc2 # Configure I2C on GPIO Pins #22 and #23 dtoverlay=i2c-gpio,i2c-gpio_sda=23,i2c_gpio_scl=22,i2c_gpio_delay_us=2 # Configure DPI on GPIO Pins #0 through #21 gpio=0=op gpio=0=pn gpio=1-27=ip gpio=1-27=pn # Enable DPI18 Overlay enable_dpi_lcd=1 display_default_lcd=1 dpi_group=2 dpi_mode=87 # Configure DPI Video Timings # RGB 666 CFG 1 (MODE 5) dpi_output_format=458773 # 58 Hz Timings (Low-End Spec) # Works at GPIO DRIVE 5-7 hdmi_timings=1920 0 20 10 10 1080 0 10 10 10 0 0 0 58 0 125000000 3 # NOTE: GPIO PINS #24 - #27 ARE DRIVEN SEPARATELY BY WiringPi SOFTWARE [pi4] # Enable DRM VC4 V3D driver on top of the dispmanx display stack #dtoverlay=vc4-fkms-v3d #max_framebuffers=2 [all] #dtoverlay=vc4-fkms-v3d
我们使用的电源来自Canakit 5.1V 3.5A,该电源在EVM用户手册中列出的建议范围内。 此外,据我所能理解,这并不能解释为什么在静态图片中显示颜色,而不是RPI界面。
Andrew