请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DLPC3478 主题中讨论的其他器件: DLPC350
数据表指出 DLPC3478的 I2C (例如 IIC0_SCL)的输入为迟滞。
但是,这种程度没有规定。
DLPC350数据表规定 VHYS (VHYS+ VT - VT)= 550mV。
DLPC3478的规格是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.