请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DLPC3479 主题中讨论的其他器件: DLPC3470、 DLPC3478
"DLPC3479软件编程人员指南(修订版 B)"的"3.4.7写入图形配置(96h)"中有4至6位说明、但 DLPC3479固件 v8.3.0版本说明中没有说明。
此致、
门胁市
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.