This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TXS0102:数据请求

Guru**** 2922540 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1505832/txs0102-data-request

器件型号:TXS0102

工具/软件:

尊敬的专家:

我对1.8V 侧(3.3 -> 1.8)的 TXS0102DQER 的 VoL max 有疑问。 数据表在1mA 输出电流下的规格为0.4V。

如果输出电流限制为1uA/10uA/100uA 且我们的最高环境温度为60C、您是否有数据说明 VoL 最大值是多少?

谢谢!

McKenna