This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS90UB948-Q1:DS90UB948-Q1

Guru**** 2589265 points
Other Parts Discussed in Thread: DS90UB949-Q1, DS90UB948-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1532696/ds90ub948-q1-ds90ub948-q1

器件型号:DS90UB948-Q1
主题中讨论的其他器件:DS90UB949-Q1

工具/软件:

当前的 FCE 需要 TI 技术团队根据这些参数提供新的配置文件)寄存器值(

到底是什么  DS90UB949-Q1  而解串器是  DS90UB948-Q1

期待您或您的团队提供反馈 。

非常感谢!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    嗨、Junxi、

    请参阅以下 949-Q1 初始化代码示例脚本、其中包括 949-Q1 器件的最新勘误表。

    """
      TI Confidential - NDA Restrictions
    
      Copyright 2020 Texas Instruments Incorporated. All rights reserved.
    
      IMPORTANT: Your use of this Software is limited to those specific rights
      granted under the terms of a software license agreement between the user who
      downloaded the software, his/her employer (which must be your employer) and
      Texas Instruments Incorporated (the "License"). You may not use this Software
      unless you agree to abide by the terms of the License. The License limits your
      use, and you acknowledge, that the Software may not be modified, copied or
      distributed unless embedded on a Texas Instruments microcontroller which is
      integrated into your product. Other than for the foregoing purpose, you may
      not use, reproduce, copy, prepare derivative works of, modify, distribute,
      perform, display or sell this Software and/or its documentation for any
      purpose.
    
      YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
      PROVIDED AS IS WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
      INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
      NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL TEXAS
      INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
      NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER LEGAL
      EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES INCLUDING BUT NOT
      LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE OR CONSEQUENTIAL
      DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT OF SUBSTITUTE GOODS,
      TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES (INCLUDING BUT NOT
      LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.
    
      Should you have any questions regarding your right to use this Software,
      contact Texas Instruments Incorporated at www.TI.com.
    
    """
    ############################
    # DS90UH949-Q1 Init Code Example v1.0
    # 949->948, Dual FPD-Link STP, 1920x720@60Hz
    ############################
    
    import time
    import sys
    
    # System dependant variables - adjust according to system 
    UB949 = 0x18        # 949 I2C Address
    UB948 = 0x68        # Remote 948 Address
    
    def pollstate():
        count=0
        board.WriteI2C(UB949,0x23,0x80)
        board.WriteI2C(UB949,0x24,0x80)
        mask = int('11111',2)
        state = board.ReadI2C(UB949,0x24,1)
        while (state & mask) != 27:   #27 = 5'b11011
            time.sleep(0.01)  #10ms delay
            state = board.ReadI2C(UB949,0x24,1)
            count = count +1
            if count == 10:
                print "Error: Serializer is not in Normal state"
                return(1)
        
        board.WriteI2C(UB949,0x23,0x0)
        board.WriteI2C(UB949,0x24,0x0)
    
            
    
    def initsequence():
    
        board.WriteI2C(UB949,0x03,0xDA) # Set I2C passthrough
        
        linked = 0
        retry = 0
        mask = int('10000000',2)
        while linked == 0:
            STS = board.ReadI2C(UB949,0x5A,1)
            if ((STS & mask) != 0):
                linked = 1
                print "Deserializer Detected"
            else:
                time.sleep(0.1)
                retry = retry + 1
                if retry == 10:
                    print "Error: No Deserializer Detected"
                    return()
    
        board.WriteI2C(UB948,0x4A,0x01) # Disable OLDI outputs on 948 to prevent screen glitches from appearing during the init process 
    
        ##### Init A Sequence
    
        # Errata #2, 3, 4
        board.WriteI2C(UB949,0x5B,0x03) # Force dual FPD-Link, disable reset on PLL frequency change 
    
        # Errata #7
        board.WriteI2C(UB949,0x16,0x02) # Adjust BCC watchdog timer to minimum
    
        state_error = pollstate()  # Poll 949 state machine prior to applying init B errata
    
        if state_error == 1:
            return()
    
        ##### Init B Sequence
    
        # Reset HDMI PLL after TMDS clock has stabilized 
        board.WriteI2C(UB949,0x40,0x10)
        board.WriteI2C(UB949,0x41,0x49)
        board.WriteI2C(UB949,0x42,0x10)
        board.WriteI2C(UB949,0x42,0x00)
    
        # Reset FPD PLL 
        board.WriteI2C(UB949,0x40,0x14)
        board.WriteI2C(UB949,0x41,0x49)
        board.WriteI2C(UB949,0x42,0x10)
        board.WriteI2C(UB949,0x42,0x00)
    
        board.WriteI2C(UB948,0x01,0x01) # Digital reset to restart AEQ 
        time.sleep(0.1) # Allow time for 948 to relock 
        board.WriteI2C(UB948,0x4A,0x00) # Enable OLDI outputs on 948
    
    initsequence()

    此代码配置为 SER 和 DES 之间的双连接、如果情况并非如此、请通知我。

    如果您有任何问题、请告诉我。

    此致、

    Miguel