This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DP83869HM:DP83869无法正确识别设置模式,且网络端口无法通信

Guru**** 2943430 points

Other Parts Discussed in Thread: USB-2-MDIO

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1065900/dp83869hm-dp83869-cannot-correctly-recognize-the-setting-mode-and-the-network-port-cannot-communicate

部件号:DP83869HM
“线程”中讨论的其它部件:USB-2-MDIODP83869

你好,支持团队

我的客户有以下问题:

此时有一个问题:连接到网线后网络端口没有响应,LED 指示灯不亮,并且没有链路连接现象。
具体分析:


1.打开 putty 串行调试助手后,进入 u-boot 调试界面并输入 MII 信息,它将显示与 phy 对应的寄存器端口是1000BASE-X,即光纤端口,而不管网线是否已连接。

Zynq> MII 信息
PHY 0x00:OUI = 0x80028,型号= 0x0F,Rev = 0x01,1000baseX,HDX
PHY 0x08:OUI = 0x0000,型号= 0x00,Rev = 0x00,10baseT,HDX

2.我在设备树中添加的配置如下:

#include <dt-bindings/net/ti-dp83869.h>
&gem1 {
gmii2rgmii-phy-handle = <&gmii_to_rgmii_0>;
phy-handle = <&phy1>;
ps7_ethernet_1_mdio: mdio {
#address-cells = <1>;
#size-cells = <0>;
phy1: phy@1 {
reg = <0>;
device_type = "ethernet-phy";
tx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
rx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
ti,op-mode = <DP83869_RGMII_COPPER_ETHERNET>;
ti,max-output-impedance = "true";
ti,clk-output-sel = <DP83869_CLK_O_SEL_CHN_A_RCLK>;
rx-internal-delay-ps = <2000>;
tx-internal-delay-ps = <2000>;
};
gmii_to_rgmii_0: phy@8{
compatible = "xlnx,gmii-to-rgmii-1.0";
device_type = "ethernet-phy";
phy-handle = <&phy1>;
reg = <8>;
};
};
};


如果未在设备树中配置,则无法识别特定的 PHY 芯片,并且在启动内核时会显示通用 phy。 在这种情况下,进入 u-boot 调试界面并输入 MII 信息,它仍显示1000BASE-X,但可以识别网络端口,LED 灯亮起,主板可以相互 ping 通,但它们无法与 PC 通信。

3.我无法通过 USB-2-MDIO 软件读取和写入其寄存器,但我通过其他方法读取和写入。 分别通过 u-boot 调试接口下的 MDIO read 命令进行读写,您可以读取通用寄存器的值;通过在 dp83869.c 驱动程序中添加 printk 命令进行读写。 以下是​​我读过的寄存器值。 通过比较手册,我们可以看到它们都是正确的寄存器值。 我配置的 RGMII 到铜选件也是正确的。 因此,1000BASE-X 的情况应该是异常的。 我能理解 RJ45无法识别并相互通信的原因吗?

0000-1140
0001-7949
0002-2000
0003-a0F1
0004-011
0005-0
0006-0064
0007-2001年
0008-0
0009-0300
000A-0
000f-F000
0010-5048
0011-0002
DP83869_TATE_STS1:0
DP83869_IO_MUX_CFG:c00
01df-DP83869_OP_MODE:40
MII_DP83869_PHYCTRL:5048
DP83869_CTRL:0
DP83869_RGMIICTL:0

可以看出 RGMII 铜缆所需的寄存器信息配置正确。 但我无法确定我使用的读写方法是完全正确的。

由于我使用的是 petalinux2019.1版本的系统,其内核版本为4.19,所以我在官方网站上的答复中只找到了适用于4.14版本内核的 dp83869驱动程序。 这是否导致了我的错误?

我的 putty 启动信息如下:

U-Boot 2019.01 (Dec 31 2021 - 08:38:35 +0000) Xilinx Zynq ZC702

CPU:   Zynq 7z020
Silicon: v3.1
Model: Zynq Zed Development Board
DRAM:  ECC disabled 512 MiB
MMC:   mmc@e0100000: 0
Loading Environment from SPI Flash... SF: Detected s25fl256s_64k with page size 256 Bytes, erase size 64 KiB, total 32 MiB
OK
In:    serial@e0001000
Out:   serial@e0001000
Err:   serial@e0001000
Model: Zynq Zed Development Board
Net:   ZYNQ GEM: e000c000, phyaddr 0, interface gmii
eth0: ethernet@e000c000
Hit any key to stop autoboot:  0
Device: mmc@e0100000
Manufacturer ID: 3
OEM: 5344
Name: SC16G
Bus Speed: 50000000
Mode : SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.8 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
4174616 bytes read in 246 ms (16.2 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Verifying Hash Integrity ... OK
   Trying 'kernel@1' kernel subimage
     Description:  Linux kernel
     Type:         Kernel Image
     Compression:  uncompressed
     Data Start:   0x100000f4
     Data Size:    4157088 Bytes = 4 MiB
     Architecture: ARM
     OS:           Linux
     Load Address: 0x00008000
     Entry Point:  0x00008000
     Hash algo:    sha1
     Hash value:   f84c4227be9a3c03c6798f14dfa1cb39ab8e30db
   Verifying Hash Integrity ... sha1+ OK
## Loading fdt from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Verifying Hash Integrity ... OK
   Trying 'fdt@system-top.dtb' fdt subimage
     Description:  Flattened Device Tree blob
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x103f7094
     Data Size:    15636 Bytes = 15.3 KiB
     Architecture: ARM
     Hash algo:    sha1
     Hash value:   918e2263cd9b3e1598a3d7409a8e7127bcdb1113
   Verifying Hash Integrity ... sha1+ OK
   Booting using the fdt blob at 0x103f7094
   Loading Kernel Image ... OK
   Loading Device Tree to 07ff9000, end 07fffd13 ... OK

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.19.0-xilinx (oe-user@oe-host) (gcc version 8.2.0 (GCC)) #1 SMP PREEMPT Fri Dec 31 08:01:27 UTC 2021
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: Zynq Zed Development Board
bootconsole [earlycon0] enabled
Memory policy: Data cache writealloc
cma: Reserved 16 MiB at 0x1f000000
random: get_random_bytes called from start_kernel+0x80/0x3c4 with crng_init=0
percpu: Embedded 16 pages/cpu @(ptrval) s35916 r8192 d21428 u65536
Built 1 zonelists, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttyPS0,115200 earlyprintk root=/dev/mmcblk0p2 rw rootwait
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 493120K/524288K available (6144K kernel code, 205K rwdata, 1616K rodata, 1024K init, 132K bss, 14784K reserved, 16384K cma-reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0x(ptrval) - 0x(ptrval)   (7136 kB)
      .init : 0x(ptrval) - 0x(ptrval)   (1024 kB)
      .data : 0x(ptrval) - 0x(ptrval)   ( 206 kB)
       .bss : 0x(ptrval) - 0x(ptrval)   ( 133 kB)
rcu: Preemptible hierarchical RCU implementation.
rcu:    RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
        Tasks RCU enabled.
rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
efuse mapped to (ptrval)
slcr mapped to (ptrval)
L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 1 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 8 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
zynq_clock_init: clkc starts at (ptrval)
Zynq clock init
sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
Switching to timer-based delay loop, resolution 3ns
clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
timer #0 at (ptrval), irq=17
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x100000 - 0x100060
rcu: Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 2 CPUs
SMP: Total of 2 processors activated (1333.33 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 512 (order: 3, 32768 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval)
zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 25, base_baud = 6249999) is a xu`▒▒k▒▒▒▒[ttyPS0] enabled
console [ttyPS0] enabled
bootconsole [earlycon0] disabled
bootconsole [earlycon0] disabled
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
media: Linux media interface: v0.10
videodev: Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
EDAC MC: Ver: 3.0.0
FPGA manager framework
Advanced Linux Sound Architecture Driver Initialized.
clocksource: Switched to clocksource arm_global_timer
NET: Registered protocol family 2
tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
workingset: timestamp_bits=30 max_order=17 bucket_order=0
jffs2: version 2.2. (NAND) (SUMMARY)  Copyright 2001-2006 Red Hat, Inc.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
dma-pl330 f8003000.dmac:        DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
brd: module loaded
loop: module loaded
m25p80 spi0.0: found s25fl256s1, expected n25q512a
m25p80 spi0.0: s25fl256s1 (32768 Kbytes)
4 fixed-partitions partitions found on MTD device spi0.0
Creating 4 MTD partitions on "spi0.0":
0x000000000000-0x000000500000 : "boot"
0x000000500000-0x000000520000 : "bootenv"
0x000000520000-0x000000fa0000 : "kernel"
0x000000fa0000-0x000002000000 : "spare"
libphy: Fixed MDIO Bus: probed
CAN device driver interface
libphy: MACB_mii_bus: probed
DP83869_STRAP_STS1:0
DP83869_IO_MUX_CFG:c00
DP83869_OP_MODE:40
MII_DP83869_PHYCTRL:5048
DP83869_CTRL:0
DP83869_RGMIICTL:0
TI DP83869 e000c000.ethernet-ffffffff:00: attached PHY driver [TI DP83869] (mii_bus:phy_addr=e000c000.ethernet-ffffffff:00, irq=POLL)
macb e000c000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000c000 irq 27 (00:0a:35:00:22:02)
e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
usbcore: registered new interface driver usb-storage
chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
chipidea-usb2 e0002000.usb: Linked as a consumer to regulator.0
ULPI transceiver vendor/product ID 0x0451/0x1507
Found TI TUSB1210 ULPI transceiver.
ULPI integrity check: passed.
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
i2c /dev entries driver
cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer at (ptrval) with timeout 10s
EDAC MC: ECC not enabled
Xilinx Zynq CpuIdle Driver started
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA
ledtrig-cpu: registered to indicate activity on CPUs
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
NET: Registered protocol family 10
Segment Routing with IPv6
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20170425 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20170425)
can: broadcast manager protocol (rev 20170425 t)
can: netlink gateway (rev 20170425) max_hops=1
Registering SWP/SWPB emulation handler
of-fpga-region fpga-full: FPGA Region probed
hctosys: unable to open rtc device (rtc0)
of_cfs_init
of_cfs_init: OK
ALSA device list:
  No soundcards found.
Waiting for root device /dev/mmcblk0p2...
mmc0: new high speed SDHC card at address aaaa
mmcblk0: mmc0:aaaa SC16G 14.8 GiB
 mmcblk0: p1 p2
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 1024K
Run /sbin/init as init process
INIT: version 2.88 booting
random: fast init done
Starting udev
udevd[747]: starting version 3.2.5
random: udevd: uninitialized urandom read (16 bytes read)
random: udevd: uninitialized urandom read (16 bytes read)
random: udevd: uninitialized urandom read (16 bytes read)
udevd[748]: starting eudev-3.2.5
ha1588: loading out-of-tree module taints kernel.
The major of the test device is 244
remap_size is 4096
res->start is 41000000
ha1588probed at VA 0xe0988000
FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
hwclock: can't open '/dev/misc/rtc': No such file or directory
Fri Dec 31 08:38:59 UTC 2021
hwclock: can't open '/dev/misc/rtc': No such file or directory
urandom_read: 2 callbacks suppressed
random: dd: uninitialized urandom read (512 bytes read)
mknod: /deb/dp83869: No such file or directory
Hello PetaLinux World
INIT: Entering runlevel: 5
Configuring network interfaces... IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
done.
Starting Dropbear SSH server: random: dropbear: uninitialized urandom read (32 bytes read)
dropbear.
hwclock: can't open '/dev/misc/rtc': No such file or directory
Starting internet superserver: inetd.
Starting syslogd/klogd: done
Starting tcf-agent: OK

PetaLinux 2019.1 wr_2 /dev/ttyPS0
wr_2 login: root
Password:
root@wr_2:~# ifconfig
eth0      Link encap:Ethernet  HWaddr 00:0A:35:00:22:02
          inet addr:192.168.0.100  Bcast:0.0.0.0  Mask:255.255.255.0
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Interrupt:27 Base address:0xc000

lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

非常感谢。

此致,
尤基

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    以下是驱动程序文件:

    e2e.ti.com/.../dp83869.c

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

     通常,板上使用带电阻器在启动时以所需模式配置设备。 客户可以检查原理图一次,以确保正在使用正确的绑带设置,以便 PHY 在所需模式下启动。 我们不确定 u-boot OS 要求和 Linux 驱动程序示例中所需的更新,因此可能无法直接识别问题的根源。 但客户可能会尝试按照软件配置强制 PHY 处于 RGMII 铜缆模式(来自数据表第9.4-8节)

    配置寄存器0x01DF 后,请执行以下操作。
    •写入0x1140以注册0x0000
    •写入0x5048以注册0x0010
    •写入0x0B00以注册0x0009"

    此致,

    维克拉姆

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,

    关于绑带信息,我确保正确配置它。 我将其功能模式的 JTAG_EDO,RX_D3和 RX_D2配置为0。 从我上面给出的寄存器信息可以看出,0x6E strap _STS 为0,表示带配置正确。 同样,我上面给出的寄存器也可以表明我已经执行了以下操作
    •写入0x1140以注册0x0000
    •写入0x5048以注册0x0010
    •写入0x0B00以注册0x0009"
    但它没有成功地让我识别以太网端口。 我是否有其他方法来验证问题在哪里?

    此致

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    齐您好,

    我将与团队进行一次核对,但根据现有数据,我无法从根本上解决问题。 也许您可以尝试启用环回并查看 是否看到链路连接(在拔下电缆后)。

    REG 数据   

    01DF 0040 //to enable RGMII to Copper mode (01DF 0040 //启用 RGMII 到铜线模式)
    00FE E720
    0000 0140
    0010 5008
    0016 0008
    001F 4000

    阅读注册表0001以了解链接状态。

    此致,

    维克拉姆