This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TCAN4550:演示代码:中断处理

Guru**** 2952510 points

Other Parts Discussed in Thread: TCAN4550

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1081210/tcan4550-demo-code-interrupt-handling

部件号:TCAN4550

e2e 团队,  

我正在尝试使用 TCAN4550的演示代码 通过推 入交换机 S1和/或 S2,在 CAN 总线上发送2个不同的 WUP (具有2个节点)。 如果我们运行演示代码,WUP 将持续传输,直到按下重置按钮。 我想要的是,只要我按下主板上的按钮 S1,就会产生中断,并且循环会运行一段有限的时间(比如10秒),然后当我再次按下按钮时,会产生另一个中断,再产生10秒 (比如)。 其目的是通过同一 S1交换机在 CAN 总线上发送不同的 WUP,以更好地控制数据的发送和定时。

随附的是主代码。  

/*
 * main.c
 * Author: Texas Instruments
 * Date: 4/25/2019
 *
 * Description: A basic version of code to set up and receive a packet.
 *  - This is designed to work with the EVM the BOOSTXL-CANFD-LIN Rev 1.0 Boosterpack
 *  - It assumes TCAN4550 Oscillator of 40 MHz
 *  - Sets CAN arbitration rate at 500 kBaud
 *  - Sets CAN FD data phase for 2 MBaud
 *  - The interrupt pin is used for signal a received message, rather than polling
 *
 *   Pressing S1 will transmit a CAN message. S1 is on the MSP430FR6989 launchpad to the left.
 *
 *  Pinout
 *   - P1.4 SPI Clock / SCLK
 *   - P1.6 MOSI / SDI
 *   - P1.7 MISO / SDO
 *   - P2.5 SPI Chip Select / nCS
 *
 *   - P2.3 MCAN Interrupt 1 / nINT
 *   - Ground wire is important
 *
 *
 *
 * Copyright (c) 2019 Texas Instruments Incorporated.  All rights reserved.
 * Software License Agreement
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * Redistributions of source code must retain the above copyright
 * notice, this list of conditions and the following disclaimer.
 *
 * Redistributions in binary form must reproduce the above copyright
 * notice, this list of conditions and the following disclaimer in the
 * documentation and/or other materials provided with the
 * distribution.
 *
 * Neither the name of Texas Instruments Incorporated nor the names of
 * its contributors may be used to endorse or promote products derived
 * from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
 * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
 * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
 * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

#include <driverlib.h>
#include <msp430.h>

#include "tcan4x5x/TCAN4550.h"


void Init_GPIO(void);
void Init_Clock(void);
void Init_SPI(void);
void Init_CAN(void);

volatile uint8_t TCAN_Int_Cnt = 0;					// A variable used to keep track of interrupts the MCAN Interrupt pin


int
main(void)
{
	/***********************************
	 * MSP430 Specific Initializations *
	 ***********************************/
	WDT_A_hold(__MSP430_BASEADDRESS_WDT_A__);
	Init_GPIO();									// Set up GPIOs for SPI and TCAN4550 connections
	Init_Clock();									// Set up the system clocks for 16 MHz (on the MSP430)
	Init_SPI();										// Initialize the SPI hardware module for 2 MHz SPI
	GPIO_clearInterrupt(GPIO_PORT_P1, GPIO_PIN1);   // Clear any interrupts on pin 1.1 before we enable global interrupts
	GPIO_clearInterrupt(GPIO_PORT_P2, GPIO_PIN3);	// Clear any interrupts on pin 2.3 before we enable global interrupts
	__enable_interrupt();


	/*********************************************
	 * Everything at this point is for TCAN4550  *
	 *********************************************/
	Init_CAN();										// Run the main MCAN configuration sequence. The bulk of the configuration is in this!

	/* Define the CAN message we want to send*/
	TCAN4x5x_MCAN_TX_Header header = {0};			// Remember to initialize to 0, or you'll get random garbage!
	uint8_t data[4] = {0x55, 0x66, 0x77, 0x88};		// Define the data payload
	header.DLC = MCAN_DLC_4B;						// Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
	header.ID = 0x144;								// Set the ID
	header.FDF = 0;									// CAN FD frame enabled
	header.BRS = 0;									// Bit rate switch enabled
	header.EFC = 0;
	header.MM  = 0;
	header.RTR = 0;
	header.XTD = 1;									// We are not using an extended ID in this example
	header.ESI = 0;									// Error state indicator


	TCAN4x5x_MCAN_WriteTXBuffer(0, &header, data);	// This function actually writes the header and data payload to the TCAN's MRAM in the specified TX queue number. It returns the bit necessary to write to TXBAR,
													// but does not necessarily require you to use it. In this example, we won't, so that we can send the data queued up at a later point.

	/* Let's make a different CAN message */
	data[0] = 0x11;
	data[1] = 0x22;
	data[2] = 0x33;
	data[3] = 0x44;									// Define the data payload

	header.DLC = MCAN_DLC_4B;						// Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
	header.ID = 0x145;								// Set the ID
	header.FDF = 0;									// CAN FD frame enabled
	header.BRS = 0;									// Bit rate switch enabled
	header.EFC = 0;
	header.MM  = 0;
	header.RTR = 0;
	header.XTD = 1;									// We are not using an extended ID in this example
	header.ESI = 0;									// Error state indicator

	TCAN4x5x_MCAN_WriteTXBuffer(1, &header, data);	// This line writes the data and header to TX FIFO 1
	//TCAN4x5x_MCAN_TransmitBufferContents(1);		// Request that TX Buffer 1 be transmitted
// commenting out transmit function calls --> we do not want to call these functions
//as we will use S1 and S2 on the board (on msp430) --> P1.1 S1, P1.2 S2
	//  TCAN4x5x_MCAN_TransmitBufferContents(0);//P1.1
//  TCAN4x5x_MCAN_TransmitBufferContents(1);  //P1.2

//	TCAN4x5x_MCAN_TransmitBufferContents(0);		// Now we can send the TX FIFO element 0 data that we had queued up earlier but didn't send.

	while (1)
	{
		if (TCAN_Int_Cnt > 0 )
		{
			TCAN_Int_Cnt--;
			TCAN4x5x_Device_Interrupts dev_ir = {0};            // Define a new Device IR object for device (non-CAN) interrupt checking
			TCAN4x5x_MCAN_Interrupts mcan_ir = {0};				// Setup a new MCAN IR object for easy interrupt checking
			TCAN4x5x_Device_ReadInterrupts(&dev_ir);            // Read the device interrupt register
			TCAN4x5x_MCAN_ReadInterrupts(&mcan_ir);		        // Read the interrupt register

			if (dev_ir.SPIERR)                                  // If the SPIERR flag is set
			    TCAN4x5x_Device_ClearSPIERR();                  // Clear the SPIERR flag

			if (mcan_ir.RF0N)									// If a new message in RX FIFO 0
			{
				TCAN4x5x_MCAN_RX_Header MsgHeader = {0};		// Initialize to 0 or you'll get garbage
				uint8_t numBytes = 0;                           // Used since the ReadNextFIFO function will return how many bytes of data were read
				uint8_t dataPayload[64] = {0};                  // Used to store the received data

				TCAN4x5x_MCAN_ClearInterrupts(&mcan_ir);	    // Clear any of the interrupt bits that are set.

				numBytes = TCAN4x5x_MCAN_ReadNextFIFO( RXFIFO0, &MsgHeader, dataPayload);	// This will read the next element in the RX FIFO 0

				// numBytes will have the number of bytes it transfered in it. Or you can decode the DLC value in MsgHeader.DLC
				// The data is now in dataPayload[], and message specific information is in the MsgHeader struct.
				if (MsgHeader.ID == 0x0AA)		// Example of how you can do an action based off a received address
				{
					// Do something
				}
			}
		}
	}
}

/*
 * Configure the TCAN4550
 */
void
Init_CAN(void)
{
    TCAN4x5x_Device_ClearSPIERR();                              // Clear any SPI ERR flags that might be set as a result of our pin mux changing during MCU startup

    /* Step one attempt to clear all interrupts */
	TCAN4x5x_Device_Interrupt_Enable dev_ie = {0};				// Initialize to 0 to all bits are set to 0.
	TCAN4x5x_Device_ConfigureInterruptEnable(&dev_ie);	        // Disable all non-MCAN related interrupts for simplicity

	TCAN4x5x_Device_Interrupts dev_ir = {0};					// Setup a new MCAN IR object for easy interrupt checking
	TCAN4x5x_Device_ReadInterrupts(&dev_ir);					// Request that the struct be updated with current DEVICE (not MCAN) interrupt values

	if (dev_ir.PWRON)                                           // If the Power On interrupt flag is set
		TCAN4x5x_Device_ClearInterrupts(&dev_ir);               // Clear it because if it's not cleared within ~4 minutes, it goes to sleep

	/* Configure the CAN bus speeds */
	TCAN4x5x_MCAN_Nominal_Timing_Simple TCANNomTiming = {0};	// 500k arbitration with a 40 MHz crystal ((40E6 / 2) / (32 + 8) = 500E3)
	TCANNomTiming.NominalBitRatePrescaler = 2;
	TCANNomTiming.NominalTqBeforeSamplePoint = 32;
	TCANNomTiming.NominalTqAfterSamplePoint = 8;

	TCAN4x5x_MCAN_Data_Timing_Simple TCANDataTiming = {0};		// 2 Mbps CAN FD with a 40 MHz crystal (40E6 / (15 + 5) = 2E6)
	TCANDataTiming.DataBitRatePrescaler = 1;
	TCANDataTiming.DataTqBeforeSamplePoint = 15;
	TCANDataTiming.DataTqAfterSamplePoint = 5;

	/* Configure the MCAN core settings */
	TCAN4x5x_MCAN_CCCR_Config cccrConfig = {0};					// Remember to initialize to 0, or you'll get random garbage!
	cccrConfig.FDOE = 1;										// CAN FD mode enable
	cccrConfig.BRSE = 1;										// CAN FD Bit rate switch enable

	/* Configure the default CAN packet filtering settings */
	TCAN4x5x_MCAN_Global_Filter_Configuration gfc = {0};
	gfc.RRFE = 1;                                               // Reject remote frames (TCAN4x5x doesn't support this)
	gfc.RRFS = 1;                                               // Reject remote frames (TCAN4x5x doesn't support this)
	gfc.ANFE = TCAN4x5x_GFC_ACCEPT_INTO_RXFIFO0;                // Default behavior if incoming message doesn't match a filter is to accept into RXFIO0 for extended ID messages (29 bit IDs)
	gfc.ANFS = TCAN4x5x_GFC_ACCEPT_INTO_RXFIFO0;                // Default behavior if incoming message doesn't match a filter is to accept into RXFIO0 for standard ID messages (11 bit IDs)

	/* ************************************************************************
	 * In the next configuration block, we will set the MCAN core up to have:
	 *   - 1 SID filter element
	 *   - 1 XID Filter element
	 *   - 5 RX FIFO 0 elements
	 *   - RX FIFO 0 supports data payloads up to 64 bytes
	 *   - RX FIFO 1 and RX Buffer will not have any elements, but we still set their data payload sizes, even though it's not required
	 *   - No TX Event FIFOs
	 *   - 2 Transmit buffers supporting up to 64 bytes of data payload
	 */
	TCAN4x5x_MRAM_Config MRAMConfiguration = {0};
	MRAMConfiguration.SIDNumElements = 1;						// Standard ID number of elements, you MUST have a filter written to MRAM for each element defined
	MRAMConfiguration.XIDNumElements = 1;						// Extended ID number of elements, you MUST have a filter written to MRAM for each element defined
	MRAMConfiguration.Rx0NumElements = 5;						// RX0 Number of elements
	MRAMConfiguration.Rx0ElementSize = MRAM_64_Byte_Data;		// RX0 data payload size
	MRAMConfiguration.Rx1NumElements = 0;						// RX1 number of elements
	MRAMConfiguration.Rx1ElementSize = MRAM_64_Byte_Data;		// RX1 data payload size
	MRAMConfiguration.RxBufNumElements = 0;						// RX buffer number of elements
	MRAMConfiguration.RxBufElementSize = MRAM_64_Byte_Data;		// RX buffer data payload size
	MRAMConfiguration.TxEventFIFONumElements = 0;				// TX Event FIFO number of elements
	MRAMConfiguration.TxBufferNumElements = 2;					// TX buffer number of elements
	MRAMConfiguration.TxBufferElementSize = MRAM_64_Byte_Data;	// TX buffer data payload size


	/* Configure the MCAN core with the settings above, the changes in this block are write protected registers,      *
	 * so it makes the most sense to do them all at once, so we only unlock and lock once                             */

	TCAN4x5x_MCAN_EnableProtectedRegisters();					// Start by making protected registers accessible
	TCAN4x5x_MCAN_ConfigureCCCRRegister(&cccrConfig);			// Enable FD mode and Bit rate switching
	TCAN4x5x_MCAN_ConfigureGlobalFilter(&gfc);                  // Configure the global filter configuration (Default CAN message behavior)
	TCAN4x5x_MCAN_ConfigureNominalTiming_Simple(&TCANNomTiming);// Setup nominal/arbitration bit timing
	TCAN4x5x_MCAN_ConfigureDataTiming_Simple(&TCANDataTiming);	// Setup CAN FD timing
	TCAN4x5x_MRAM_Clear();										// Clear all of MRAM (Writes 0's to all of it)
	TCAN4x5x_MRAM_Configure(&MRAMConfiguration);				// Set up the applicable registers related to MRAM configuration
	TCAN4x5x_MCAN_DisableProtectedRegisters();					// Disable protected write and take device out of INIT mode


	/* Set the interrupts we want to enable for MCAN */
	TCAN4x5x_MCAN_Interrupt_Enable mcan_ie = {0};				// Remember to initialize to 0, or you'll get random garbage!
	mcan_ie.RF0NE = 1;											// RX FIFO 0 new message interrupt enable

	TCAN4x5x_MCAN_ConfigureInterruptEnable(&mcan_ie);			// Enable the appropriate registers


	/* Setup filters, this filter will mark any message with ID 0x055 as a priority message */
	TCAN4x5x_MCAN_SID_Filter SID_ID = {0};
	SID_ID.SFT = TCAN4x5x_SID_SFT_CLASSIC;						// SFT: Standard filter type. Configured as a classic filter
	SID_ID.SFEC = TCAN4x5x_SID_SFEC_PRIORITYSTORERX0;			// Standard filter element configuration, store it in RX fifo 0 as a priority message
	SID_ID.SFID1 = 0x055;										// SFID1 (Classic mode Filter)
	SID_ID.SFID2 = 0x7FF;										// SFID2 (Classic mode Mask)
	TCAN4x5x_MCAN_WriteSIDFilter(0, &SID_ID);					// Write to the MRAM


	/* Store ID 0x12345678 as a priority message */
	TCAN4x5x_MCAN_XID_Filter XID_ID = {0};
	XID_ID.EFT = TCAN4x5x_XID_EFT_CLASSIC;                      // EFT
	XID_ID.EFEC = TCAN4x5x_XID_EFEC_PRIORITYSTORERX0;           // EFEC
	XID_ID.EFID1 = 0x12345678;                                  // EFID1 (Classic mode filter)
	XID_ID.EFID2 = 0x1FFFFFFF;                                  // EFID2 (Classic mode mask)
	TCAN4x5x_MCAN_WriteXIDFilter(0, &XID_ID);                   // Write to the MRAM

	/* Configure the TCAN4550 Non-CAN-related functions */
	TCAN4x5x_DEV_CONFIG devConfig = {0};                        // Remember to initialize to 0, or you'll get random garbage!
	devConfig.SWE_DIS = 0;                                      // Keep Sleep Wake Error Enabled (it's a disable bit, not an enable)
	devConfig.DEVICE_RESET = 0;                                 // Not requesting a software reset
	devConfig.WD_EN = 0;                                        // Watchdog disabled
	devConfig.nWKRQ_CONFIG = 0;                                 // Mirror INH function (default)
	devConfig.INH_DIS = 0;                                      // INH enabled (default)
	devConfig.GPIO1_GPO_CONFIG = TCAN4x5x_DEV_CONFIG_GPO1_MCAN_INT1;    // MCAN nINT 1 (default)
	devConfig.FAIL_SAFE_EN = 0;                                 // Failsafe disabled (default)
	devConfig.GPIO1_CONFIG = TCAN4x5x_DEV_CONFIG_GPIO1_CONFIG_GPO;      // GPIO set as GPO (Default)
	devConfig.WD_ACTION = TCAN4x5x_DEV_CONFIG_WDT_ACTION_nINT;  // Watchdog set an interrupt (default)
	devConfig.WD_BIT_RESET = 0;                                 // Don't reset the watchdog
	devConfig.nWKRQ_VOLTAGE = 0;                                // Set nWKRQ to internal voltage rail (default)
	devConfig.GPO2_CONFIG = TCAN4x5x_DEV_CONFIG_GPO2_NO_ACTION; // GPO2 has no behavior (default)
	devConfig.CLK_REF = 1;                                      // Input crystal is a 40 MHz crystal (default)
	devConfig.WAKE_CONFIG = TCAN4x5x_DEV_CONFIG_WAKE_BOTH_EDGES;// Wake pin can be triggered by either edge (default)
	TCAN4x5x_Device_Configure(&devConfig);                      // Configure the device with the above configuration

	TCAN4x5x_Device_SetMode(TCAN4x5x_DEVICE_MODE_NORMAL);       // Set to normal mode, since configuration is done. This line turns on the transceiver

	TCAN4x5x_MCAN_ClearInterruptsAll();                         // Resets all MCAN interrupts (does NOT include any SPIERR interrupts)
}


/*
 * GPIO Initialization
 */
void
Init_GPIO()
{
	// Set all GPIO pins to output low to prevent floating input and reduce power consumption
	GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P4, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P5, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P6, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P7, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P8, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setOutputLowOnPin(GPIO_PORT_P9, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);

	GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P2, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P3, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P4, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P5, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P6, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P7, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P8, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
	GPIO_setAsOutputPin(GPIO_PORT_P9, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);


	// Set P3.2 as input with weak pull up since this is GPIO1
	GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P3, GPIO_PIN2);

	// Set P3.1 as input for GPO2
	GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P3, GPIO_PIN1);

	// Set P2.1 as input with weak pull up since this is GPO2
	GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P2, GPIO_PIN1);


	// Configure P1.1 interrupt for S1 (left button on launchpad)
	GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1);
	GPIO_selectInterruptEdge(GPIO_PORT_P1, GPIO_PIN1, GPIO_HIGH_TO_LOW_TRANSITION);
	GPIO_clearInterrupt(GPIO_PORT_P1, GPIO_PIN1);
	GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN1);


	// Configure P2.3 interrupt for MCAN Interrupt 1
	GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P2, GPIO_PIN3);
	GPIO_selectInterruptEdge(GPIO_PORT_P2, GPIO_PIN3, GPIO_HIGH_TO_LOW_TRANSITION);
	GPIO_clearInterrupt(GPIO_PORT_P2, GPIO_PIN3);
	GPIO_enableInterrupt(GPIO_PORT_P2, GPIO_PIN3);

	// Set P4.1 and P4.2 as Secondary Module Function Input, LFXT.
	GPIO_setAsPeripheralModuleFunctionInputPin(
		GPIO_PORT_PJ,
		GPIO_PIN4 + GPIO_PIN5,
		GPIO_PRIMARY_MODULE_FUNCTION
	);

	/*********************************************************
	 * 					SPI Interface Pins
	 *********************************************************/
	//P1.4(SPI CLK on UCB0CLK)
	GPIO_setAsPeripheralModuleFunctionOutputPin(
		GPIO_PORT_P1,
		GPIO_PIN4,
		GPIO_PRIMARY_MODULE_FUNCTION
	);

	//P1.6(MOSI on UCB0SIMO)
	GPIO_setAsPeripheralModuleFunctionOutputPin(
		GPIO_PORT_P1,
		GPIO_PIN6,
		GPIO_PRIMARY_MODULE_FUNCTION
	);

	//P1.7(MISO on UCB0SOMI)
	GPIO_setAsPeripheralModuleFunctionInputPin(
		GPIO_PORT_P1,
		GPIO_PIN7,
		GPIO_PRIMARY_MODULE_FUNCTION
	);

	//set P2.5 as SPI CS, already set to output above
	GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN5);
	GPIO_setOutputHighOnPin(GPIO_PORT_P2, GPIO_PIN5);

	// Disable the GPIO power-on default high-impedance mode
	// to activate previously configured port settings
	PMM_unlockLPM5();
}

/*
 * Clock System Initialization
 */
void Init_Clock()
{
	// Set DCO frequency to default 8MHz
	CS_setDCOFreq(CS_DCORSEL_0, CS_DCOFSEL_6);

	// Configure MCLK and SMCLK to 8MHz
	CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);
	CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);

	// Initializes the XT1 crystal oscillator
	CS_turnOnLFXT(CS_LFXT_DRIVE_3);
}


/*
 * Initialize the EUSCI B SPI
 */
void Init_SPI()
{
	struct EUSCI_B_SPI_initMasterParam SPIParam = {0};

	SPIParam.selectClockSource=EUSCI_B_SPI_CLOCKSOURCE_SMCLK;
	SPIParam.clockSourceFrequency=8000000;
	SPIParam.desiredSpiClock=2000000;
	SPIParam.msbFirst=EUSCI_B_SPI_MSB_FIRST;
	SPIParam.clockPhase=EUSCI_B_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT;
	SPIParam.clockPolarity=EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_LOW;
	SPIParam.spiMode=EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_HIGH;


	EUSCI_B_SPI_initMaster(EUSCI_B0_BASE, &SPIParam);
	EUSCI_B_SPI_select4PinFunctionality(EUSCI_B0_BASE,0x00);

	EUSCI_B_SPI_enable(EUSCI_B0_BASE);
}


/*
 * PORT1 Interrupt Service Routine
 * Handles Interrupt from the TCAN4550 on P2.3
 */
#pragma vector = PORT1_VECTOR
__interrupt void PORT1_ISR(void)
{
    switch(__even_in_range(P1IV, P1IV_P1IFG7))
    {
    case P1IV_NONE : break;
    case P1IV_P1IFG0 : break;
    case P1IV_P1IFG1 :
        TCAN4x5x_MCAN_TransmitBufferContents(0);            // Transmits the contents of TX queue index 0 when S1 (P1.1) is pressed  --> Transmit buffer 0 (ID=0x144)
        break;
    case P1IV_P1IFG2 :
        TCAN4x5x_MCAN_TransmitBufferContents(1);     //Transmit buffer 1 (ID=0x145) when S2 is pressed
        break;
    case P1IV_P1IFG3 : break;
    case P1IV_P1IFG4 : break;
    case P1IV_P1IFG5 : break;
    case P1IV_P1IFG6 : break;
    case P1IV_P1IFG7 : break;
    }
}

/*
 * PORT2 Interrupt Service Routine
 * Handles Interrupt from the TCAN4550 on P2.3
 */
#pragma vector = PORT2_VECTOR
__interrupt void PORT2_ISR(void)
{
	switch(__even_in_range(P2IV, P2IV_P2IFG7))
	{
	case P2IV_NONE : break;
	case P2IV_P2IFG0 : break;
	case P2IV_P2IFG1 : break;
	case P2IV_P2IFG2 : break;
	case P2IV_P2IFG3 : TCAN_Int_Cnt++; break;
	case P2IV_P2IFG4 : break;
	case P2IV_P2IFG5 : break;
	case P2IV_P2IFG6 : break;
	case P2IV_P2IFG7 : break;
	}
}

在这方面,任何援助都将受到高度赞赏。  

谢谢你,

阿努布

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,阿努布,

    按下 S1开关时,TCAN4550和演示代码将尝试传输消息,直到消息成功传输并根据 CAN 协议在 CAN 总线上确认。  一旦总线上的另一个设备处于活动状态并且能够确认 CAN 消息,TCAN4550将停止尝试重新传输消息。  因为您说必须按重置按钮才能使此消息停止传输,所以总线上的其他节点可能会出现问题,无法唤醒您正在尝试传输的 WUP 消息。

    如果要禁用未确认消息的自动重传,可以将控制寄存器中的 DAR 位(0x1018,位[6])设置为“1”。  这将导致消息传输一次,仅传输一次,而不管是否已成功确认。

    通过设置 DAR 位,您可以控制消息的发送时间和发送次数,因为每次传输都需要通过 SPI 写入 TXBAR 寄存器(0x10D0)来写入相应的 TX 消息缓冲区。

    此致,

    乔纳森