This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS90UB949A-Q1:使用DS90UB948进行利润分析

Guru**** 2939240 points

Other Parts Discussed in Thread: ALP

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1086139/ds90ub949a-q1-margin-analysis-with-ds90ub948

部件号:DS90UB949A-Q1
主题中讨论的其他部件:Alp.

大家好,

为了验证余量,我们在同轴电缆的端口0和串行器输出端口1中使用了6dB衰减器。  

在6dB处,反序列化器无法使用序列化器锁定。 请查找屏幕截图。

但我们在GUI中选中了"禁用远程EDID加载"框

之后,链路打开,并显示6dB衰减器上的反序列化器和更多值。

这是我的寄存器转储,具有6dB衰减器工作和非工作状态。

请指出这背后的原因是什么,为什么利润率会增加?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    [REGISTERS]
    Device = ALP Nano 1 - DS90UB949, Connector 1
    Comments = "cid register dump with 6db att with issue condition"
    Date = 03/17/2022
    Time = 18:02:52
    Reg = 0,0x0000,0x18
    Reg = 0,0x0001,0x00
    Reg = 0,0x0003,0xDA
    Reg = 0,0x0004,0x80
    Reg = 0,0x0005,0x00
    Reg = 0,0x0006,0x00
    Reg = 0,0x0007,0x00
    Reg = 0,0x0008,0x00
    Reg = 0,0x0009,0x00
    Reg = 0,0x000A,0x00
    Reg = 0,0x000B,0x00
    Reg = 0,0x000C,0x00
    Reg = 0,0x000D,0x25
    Reg = 0,0x000E,0x33
    Reg = 0,0x000F,0x03
    Reg = 0,0x0010,0x00
    Reg = 0,0x0011,0x00
    Reg = 0,0x0012,0x00
    Reg = 0,0x0013,0xA8
    Reg = 0,0x0014,0x00
    Reg = 0,0x0015,0x01
    Reg = 0,0x0016,0x02
    Reg = 0,0x0017,0x9E
    Reg = 0,0x0018,0x7F
    Reg = 0,0x0019,0x7F
    Reg = 0,0x001A,0x01
    Reg = 0,0x001B,0x00
    Reg = 0,0x001C,0x0E
    Reg = 0,0x001D,0x00
    Reg = 0,0x001E,0x05
    Reg = 0,0x001F,0xFB
    Reg = 0,0x0020,0x00
    Reg = 0,0x0021,0x00
    Reg = 0,0x0022,0x25
    Reg = 0,0x0023,0x00
    Reg = 0,0x0024,0x00
    Reg = 0,0x0025,0x00
    Reg = 0,0x0026,0x00
    Reg = 0,0x0027,0x00
    Reg = 0,0x0028,0x01
    Reg = 0,0x0029,0x20
    Reg = 0,0x002A,0x20
    Reg = 0,0x002B,0xA0
    Reg = 0,0x002C,0x00
    Reg = 0,0x0030,0x00
    Reg = 0,0x0031,0x00
    Reg = 0,0x0032,0x00
    Reg = 0,0x0033,0x00
    Reg = 0,0x0034,0x00
    Reg = 0,0x0035,0x00
    Reg = 0,0x0036,0x00
    Reg = 0,0x0037,0x00
    Reg = 0,0x0038,0x00
    Reg = 0,0x0039,0x00
    Reg = 0,0x003A,0x00
    Reg = 0,0x003B,0x00
    Reg = 0,0x003C,0x00
    Reg = 0,0x003D,0x00
    Reg = 0,0x003E,0x00
    Reg = 0,0x003F,0x00
    Reg = 0,0x0040,0x14
    Reg = 0,0x0041,0x5C
    Reg = 0,0x0042,0x00
    Reg = 0,0x0043,0x00
    Reg = 0,0x0044,0x80
    Reg = 0,0x0045,0x00
    Reg = 0,0x0046,0x00
    Reg = 0,0x0047,0x00
    Reg = 0,0x0048,0x01
    Reg = 0,0x0049,0x68
    Reg = 0,0x004A,0x01
    Reg = 0,0x004B,0x00
    Reg = 0,0x004C,0x00
    Reg = 0,0x004D,0x00
    Reg = 0,0x004E,0x00
    Reg = 0,0x004F,0x00
    Reg = 0,0x0050,0x97
    Reg = 0,0x0051,0xA1
    Reg = 0,0x0052,0x1E
    Reg = 0,0x0053,0x00
    Reg = 0,0x0054,0x28
    Reg = 0,0x0055,0x0C
    Reg = 0,0x0056,0x00
    Reg = 0,0x0057,0x00
    Reg = 0,0x0058,0x00
    Reg = 0,0x0059,0x00
    Reg = 0,0x005A,0x02
    Reg = 0,0x005B,0x80
    Reg = 0,0x005C,0x02
    Reg = 0,0x005D,0x06
    Reg = 0,0x005E,0x44
    Reg = 0,0x005F,0x00
    Reg = 0,0x0060,0x22
    Reg = 0,0x0061,0x02
    Reg = 0,0x0062,0x00
    Reg = 0,0x0064,0x10
    Reg = 0,0x0065,0x00
    Reg = 0,0x0066,0x00
    Reg = 0,0x0067,0x00
    Reg = 0,0x0068,0x00
    Reg = 0,0x0069,0x00
    Reg = 0,0x006A,0x00
    Reg = 0,0x006B,0x00
    Reg = 0,0x006C,0x00
    Reg = 0,0x0070,0x00
    Reg = 0,0x0071,0x00
    Reg = 0,0x0072,0x00
    Reg = 0,0x0073,0x00
    Reg = 0,0x0074,0x00
    Reg = 0,0x0075,0x00
    Reg = 0,0x0076,0x00
    Reg = 0,0x0077,0x00
    Reg = 0,0x0078,0x00
    Reg = 0,0x0079,0x00
    Reg = 0,0x007A,0x00
    Reg = 0,0x007B,0x00
    Reg = 0,0x007C,0x00
    Reg = 0,0x007D,0x00
    Reg = 0,0x0080,0x00
    Reg = 0,0x0081,0x00
    Reg = 0,0x0082,0x00
    Reg = 0,0x0083,0x00
    Reg = 0,0x0084,0x00
    Reg = 0,0x0090,0x00
    Reg = 0,0x0091,0x00
    Reg = 0,0x0092,0x00
    Reg = 0,0x0093,0x00
    Reg = 0,0x0094,0x00
    Reg = 0,0x0098,0x00
    Reg = 0,0x0099,0x00
    Reg = 0,0x009A,0x00
    Reg = 0,0x009B,0x00
    Reg = 0,0x009C,0x00
    Reg = 0,0x009D,0x00
    Reg = 0,0x009E,0x00
    Reg = 0,0x009F,0x00
    Reg = 0,0x00A0,0x00
    Reg = 0,0x00A1,0x00
    Reg = 0,0x00A2,0x00
    Reg = 0,0x00A3,0x00
    Reg = 0,0x00C0,0x00
    Reg = 0,0x00C1,0x00
    Reg = 0,0x00C2,0xA8
    Reg = 0,0x00C3,0x00
    Reg = 0,0x00C4,0x40
    Reg = 0,0x00C5,0x38
    Reg = 0,0x00C6,0x00
    Reg = 0,0x00C7,0x00
    Reg = 0,0x00C8,0xC0
    Reg = 0,0x00C9,0x00
    Reg = 0,0x00CA,0x00
    Reg = 0,0x00CB,0x00
    Reg = 0,0x00CC,0x00
    Reg = 0,0x00CE,0xFF
    Reg = 0,0x00D0,0x00
    Reg = 0,0x00D1,0x00
    Reg = 0,0x00D2,0x00
    Reg = 0,0x00D3,0x00
    Reg = 0,0x00E0,0x00
    Reg = 0,0x00E1,0x00
    Reg = 0,0x00E2,0xA8
    Reg = 0,0x00E3,0x00
    Reg = 0,0x00E4,0x40
    Reg = 0,0x00E5,0x38
    Reg = 0,0x00E6,0x00
    Reg = 0,0x00E7,0x00
    Reg = 0,0x00F0,0x5F
    Reg = 0,0x00F1,0x55
    Reg = 0,0x00F2,0x42
    Reg = 0,0x00F3,0x39
    Reg = 0,0x00F4,0x34
    Reg = 0,0x00F5,0x39
    Reg = 0,0x00F6,0x00
    Reg = 0,0x00F8,0x00
    Reg = 0,0x00F9,0x00
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    [REGISTERS]
    Device = ALP Nano 1 - DS90UB949, Connector 1
    Comments = "cid-0db-att-working condition"
    Date = 03/17/2022
    Time = 18:42:14
    Reg = 0,0x0000,0x18
    Reg = 0,0x0001,0x00
    Reg = 0,0x0003,0xDA
    Reg = 0,0x0004,0x80
    Reg = 0,0x0005,0x00
    Reg = 0,0x0006,0x68
    Reg = 0,0x0007,0xA0
    Reg = 0,0x0008,0xB0
    Reg = 0,0x0009,0x00
    Reg = 0,0x000A,0x1A
    Reg = 0,0x000B,0x00
    Reg = 0,0x000C,0x07
    Reg = 0,0x000D,0x25
    Reg = 0,0x000E,0x33
    Reg = 0,0x000F,0x03
    Reg = 0,0x0010,0x00
    Reg = 0,0x0011,0x00
    Reg = 0,0x0012,0x00
    Reg = 0,0x0013,0xA8
    Reg = 0,0x0014,0x00
    Reg = 0,0x0015,0x01
    Reg = 0,0x0016,0x02
    Reg = 0,0x0017,0x9E
    Reg = 0,0x0018,0x7F
    Reg = 0,0x0019,0x7F
    Reg = 0,0x001A,0x01
    Reg = 0,0x001B,0x00
    Reg = 0,0x001C,0x0E
    Reg = 0,0x001D,0x00
    Reg = 0,0x001E,0x05
    Reg = 0,0x001F,0xF3
    Reg = 0,0x0020,0x0B
    Reg = 0,0x0021,0x00
    Reg = 0,0x0022,0x25
    Reg = 0,0x0023,0x00
    Reg = 0,0x0024,0x00
    Reg = 0,0x0025,0x00
    Reg = 0,0x0026,0x00
    Reg = 0,0x0027,0x00
    Reg = 0,0x0028,0x01
    Reg = 0,0x0029,0x20
    Reg = 0,0x002A,0x20
    Reg = 0,0x002B,0xA0
    Reg = 0,0x002C,0x00
    Reg = 0,0x0030,0x00
    Reg = 0,0x0031,0x00
    Reg = 0,0x0032,0x00
    Reg = 0,0x0033,0x00
    Reg = 0,0x0034,0x00
    Reg = 0,0x0035,0x00
    Reg = 0,0x0036,0x00
    Reg = 0,0x0037,0x00
    Reg = 0,0x0038,0x00
    Reg = 0,0x0039,0x00
    Reg = 0,0x003A,0x00
    Reg = 0,0x003B,0x00
    Reg = 0,0x003C,0x00
    Reg = 0,0x003D,0x00
    Reg = 0,0x003E,0x00
    Reg = 0,0x003F,0x00
    Reg = 0,0x0040,0x14
    Reg = 0,0x0041,0x49
    Reg = 0,0x0042,0x00
    Reg = 0,0x0043,0x00
    Reg = 0,0x0044,0x80
    Reg = 0,0x0045,0x00
    Reg = 0,0x0046,0x00
    Reg = 0,0x0047,0x00
    Reg = 0,0x0048,0x01
    Reg = 0,0x0049,0x68
    Reg = 0,0x004A,0x01
    Reg = 0,0x004B,0x56
    Reg = 0,0x004C,0x06
    Reg = 0,0x004D,0x00
    Reg = 0,0x004E,0x00
    Reg = 0,0x004F,0x00
    Reg = 0,0x0050,0x97
    Reg = 0,0x0051,0xA1
    Reg = 0,0x0052,0x1E
    Reg = 0,0x0053,0x00
    Reg = 0,0x0054,0x28
    Reg = 0,0x0055,0x0C
    Reg = 0,0x0056,0x00
    Reg = 0,0x0057,0x00
    Reg = 0,0x0058,0x00
    Reg = 0,0x0059,0x00
    Reg = 0,0x005A,0xCD
    Reg = 0,0x005B,0x80
    Reg = 0,0x005C,0x02
    Reg = 0,0x005D,0x06
    Reg = 0,0x005E,0x44
    Reg = 0,0x005F,0x8D
    Reg = 0,0x0060,0x22
    Reg = 0,0x0061,0x02
    Reg = 0,0x0062,0x00
    Reg = 0,0x0064,0x10
    Reg = 0,0x0065,0x00
    Reg = 0,0x0066,0x00
    Reg = 0,0x0067,0x00
    Reg = 0,0x0068,0x00
    Reg = 0,0x0069,0x00
    Reg = 0,0x006A,0x00
    Reg = 0,0x006B,0x00
    Reg = 0,0x006C,0x00
    Reg = 0,0x0070,0x00
    Reg = 0,0x0071,0x00
    Reg = 0,0x0072,0x00
    Reg = 0,0x0073,0x00
    Reg = 0,0x0074,0x00
    Reg = 0,0x0075,0x00
    Reg = 0,0x0076,0x00
    Reg = 0,0x0077,0x00
    Reg = 0,0x0078,0x00
    Reg = 0,0x0079,0x00
    Reg = 0,0x007A,0x00
    Reg = 0,0x007B,0x00
    Reg = 0,0x007C,0x00
    Reg = 0,0x007D,0x00
    Reg = 0,0x0080,0x00
    Reg = 0,0x0081,0x00
    Reg = 0,0x0082,0x00
    Reg = 0,0x0083,0x00
    Reg = 0,0x0084,0x00
    Reg = 0,0x0090,0x00
    Reg = 0,0x0091,0x00
    Reg = 0,0x0092,0x00
    Reg = 0,0x0093,0x00
    Reg = 0,0x0094,0x00
    Reg = 0,0x0098,0x00
    Reg = 0,0x0099,0x00
    Reg = 0,0x009A,0x00
    Reg = 0,0x009B,0x00
    Reg = 0,0x009C,0x00
    Reg = 0,0x009D,0x00
    Reg = 0,0x009E,0x00
    Reg = 0,0x009F,0x00
    Reg = 0,0x00A0,0x00
    Reg = 0,0x00A1,0x00
    Reg = 0,0x00A2,0x00
    Reg = 0,0x00A3,0x00
    Reg = 0,0x00C0,0x00
    Reg = 0,0x00C1,0x00
    Reg = 0,0x00C2,0xA8
    Reg = 0,0x00C3,0x00
    Reg = 0,0x00C4,0x68
    Reg = 0,0x00C5,0x38
    Reg = 0,0x00C6,0x00
    Reg = 0,0x00C7,0x00
    Reg = 0,0x00C8,0xC0
    Reg = 0,0x00C9,0x00
    Reg = 0,0x00CA,0x00
    Reg = 0,0x00CB,0x00
    Reg = 0,0x00CC,0x00
    Reg = 0,0x00CE,0xFF
    Reg = 0,0x00D0,0x00
    Reg = 0,0x00D1,0x00
    Reg = 0,0x00D2,0x00
    Reg = 0,0x00D3,0x00
    Reg = 0,0x00E0,0x00
    Reg = 0,0x00E1,0x00
    Reg = 0,0x00E2,0xA8
    Reg = 0,0x00E3,0x00
    Reg = 0,0x00E4,0x68
    Reg = 0,0x00E5,0x38
    Reg = 0,0x00E6,0x00
    Reg = 0,0x00E7,0x00
    Reg = 0,0x00F0,0x5F
    Reg = 0,0x00F1,0x55
    Reg = 0,0x00F2,0x42
    Reg = 0,0x00F3,0x39
    Reg = 0,0x00F4,0x34
    Reg = 0,0x00F5,0x39
    Reg = 0,0x00F6,0x00
    Reg = 0,0x00F8,0x00
    Reg = 0,0x00F9,0x00
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    # 6dB attenuator - "Disable EDID_checked condition"
    [REGISTERS]
    Device = ALP Nano 1 - DS90UB949, Connector 1
    Comments = "cid-6db-att-working condition"
    Date = 03/17/2022
    Time = 18:55:18
    Reg = 0,0x0000,0x18
    Reg = 0,0x0001,0x00
    Reg = 0,0x0003,0xDA
    Reg = 0,0x0004,0x80
    Reg = 0,0x0005,0x00
    Reg = 0,0x0006,0x68
    Reg = 0,0x0007,0x00
    Reg = 0,0x0008,0x00
    Reg = 0,0x0009,0x00
    Reg = 0,0x000A,0x0E
    Reg = 0,0x000B,0x00
    Reg = 0,0x000C,0x07
    Reg = 0,0x000D,0x25
    Reg = 0,0x000E,0x33
    Reg = 0,0x000F,0x03
    Reg = 0,0x0010,0x00
    Reg = 0,0x0011,0x00
    Reg = 0,0x0012,0x00
    Reg = 0,0x0013,0xA8
    Reg = 0,0x0014,0x00
    Reg = 0,0x0015,0x01
    Reg = 0,0x0016,0x02
    Reg = 0,0x0017,0x9E
    Reg = 0,0x0018,0x7F
    Reg = 0,0x0019,0x7F
    Reg = 0,0x001A,0x01
    Reg = 0,0x001B,0x00
    Reg = 0,0x001C,0x0E
    Reg = 0,0x001D,0x00
    Reg = 0,0x001E,0x05
    Reg = 0,0x001F,0xF3
    Reg = 0,0x0020,0x0B
    Reg = 0,0x0021,0x00
    Reg = 0,0x0022,0x25
    Reg = 0,0x0023,0x00
    Reg = 0,0x0024,0x00
    Reg = 0,0x0025,0x00
    Reg = 0,0x0026,0x00
    Reg = 0,0x0027,0x00
    Reg = 0,0x0028,0x01
    Reg = 0,0x0029,0x20
    Reg = 0,0x002A,0x20
    Reg = 0,0x002B,0xA0
    Reg = 0,0x002C,0x00
    Reg = 0,0x0030,0x00
    Reg = 0,0x0031,0x00
    Reg = 0,0x0032,0x00
    Reg = 0,0x0033,0x00
    Reg = 0,0x0034,0x00
    Reg = 0,0x0035,0x00
    Reg = 0,0x0036,0x00
    Reg = 0,0x0037,0x00
    Reg = 0,0x0038,0x00
    Reg = 0,0x0039,0x00
    Reg = 0,0x003A,0x00
    Reg = 0,0x003B,0x00
    Reg = 0,0x003C,0x00
    Reg = 0,0x003D,0x00
    Reg = 0,0x003E,0x00
    Reg = 0,0x003F,0x00
    Reg = 0,0x0040,0x14
    Reg = 0,0x0041,0x4E
    Reg = 0,0x0042,0x00
    Reg = 0,0x0043,0x00
    Reg = 0,0x0044,0x80
    Reg = 0,0x0045,0x00
    Reg = 0,0x0046,0x00
    Reg = 0,0x0047,0x00
    Reg = 0,0x0048,0x01
    Reg = 0,0x0049,0x68
    Reg = 0,0x004A,0x01
    Reg = 0,0x004B,0x56
    Reg = 0,0x004C,0x06
    Reg = 0,0x004D,0x00
    Reg = 0,0x004E,0x00
    Reg = 0,0x004F,0x00
    Reg = 0,0x0050,0x97
    Reg = 0,0x0051,0xA1
    Reg = 0,0x0052,0x1E
    Reg = 0,0x0053,0x00
    Reg = 0,0x0054,0x20
    Reg = 0,0x0055,0x0C
    Reg = 0,0x0056,0x00
    Reg = 0,0x0057,0x00
    Reg = 0,0x0058,0x00
    Reg = 0,0x0059,0x00
    Reg = 0,0x005A,0xCD
    Reg = 0,0x005B,0x00
    Reg = 0,0x005C,0x02
    Reg = 0,0x005D,0x06
    Reg = 0,0x005E,0x44
    Reg = 0,0x005F,0x8D
    Reg = 0,0x0060,0x22
    Reg = 0,0x0061,0x02
    Reg = 0,0x0062,0x00
    Reg = 0,0x0064,0x10
    Reg = 0,0x0065,0x00
    Reg = 0,0x0066,0x00
    Reg = 0,0x0067,0x00
    Reg = 0,0x0068,0x00
    Reg = 0,0x0069,0x00
    Reg = 0,0x006A,0x00
    Reg = 0,0x006B,0x00
    Reg = 0,0x006C,0x00
    Reg = 0,0x0070,0x00
    Reg = 0,0x0071,0x00
    Reg = 0,0x0072,0x00
    Reg = 0,0x0073,0x00
    Reg = 0,0x0074,0x00
    Reg = 0,0x0075,0x00
    Reg = 0,0x0076,0x00
    Reg = 0,0x0077,0x00
    Reg = 0,0x0078,0x00
    Reg = 0,0x0079,0x00
    Reg = 0,0x007A,0x00
    Reg = 0,0x007B,0x00
    Reg = 0,0x007C,0x00
    Reg = 0,0x007D,0x00
    Reg = 0,0x0080,0x00
    Reg = 0,0x0081,0x00
    Reg = 0,0x0082,0x00
    Reg = 0,0x0083,0x00
    Reg = 0,0x0084,0x00
    Reg = 0,0x0090,0x00
    Reg = 0,0x0091,0x00
    Reg = 0,0x0092,0x00
    Reg = 0,0x0093,0x00
    Reg = 0,0x0094,0x00
    Reg = 0,0x0098,0x00
    Reg = 0,0x0099,0x00
    Reg = 0,0x009A,0x00
    Reg = 0,0x009B,0x00
    Reg = 0,0x009C,0x00
    Reg = 0,0x009D,0x00
    Reg = 0,0x009E,0x00
    Reg = 0,0x009F,0x00
    Reg = 0,0x00A0,0x00
    Reg = 0,0x00A1,0x00
    Reg = 0,0x00A2,0x00
    Reg = 0,0x00A3,0x00
    Reg = 0,0x00C0,0x05
    Reg = 0,0x00C1,0x00
    Reg = 0,0x00C2,0x88
    Reg = 0,0x00C3,0x00
    Reg = 0,0x00C4,0x28
    Reg = 0,0x00C5,0x38
    Reg = 0,0x00C6,0x00
    Reg = 0,0x00C7,0x00
    Reg = 0,0x00C8,0xC0
    Reg = 0,0x00C9,0x00
    Reg = 0,0x00CA,0x00
    Reg = 0,0x00CB,0x00
    Reg = 0,0x00CC,0x00
    Reg = 0,0x00CE,0xFF
    Reg = 0,0x00D0,0x10
    Reg = 0,0x00D1,0x00
    Reg = 0,0x00D2,0x00
    Reg = 0,0x00D3,0x00
    Reg = 0,0x00E0,0x05
    Reg = 0,0x00E1,0x00
    Reg = 0,0x00E2,0x88
    Reg = 0,0x00E3,0x00
    Reg = 0,0x00E4,0x28
    Reg = 0,0x00E5,0x38
    Reg = 0,0x00E6,0x00
    Reg = 0,0x00E7,0x00
    Reg = 0,0x00F0,0x5F
    Reg = 0,0x00F1,0x55
    Reg = 0,0x00F2,0x42
    Reg = 0,0x00F3,0x39
    Reg = 0,0x00F4,0x34
    Reg = 0,0x00F5,0x39
    Reg = 0,0x00F6,0x00
    Reg = 0,0x00F8,0x00
    Reg = 0,0x00F9,0x00
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selvakumar:  

    此设置与链路边界无关,因此这可能是ALP设备检测/I2C问题,也可能是您禁用EDID检查后检测到锁定的巧合。  

    执行新的电源循环时,此行为是否可重复?  

    我将仔细检查寄存器转储中是否存在任何锁定相关性或其他明显的锁定报告问题。 下周初,我会向您提供进一步的反馈。  

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    我在选中“禁用EDID”复选框条件后确认了此行为。

    是的,它可重复多次。

    我猜在禁用EDID期间,0x5B寄存器从80更改为00。

    将更改为同轴电缆至STP模式。

    是否增加了端口0/1输出的振幅?

    谢谢

    塞尔瓦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    我们测量了该条件下的振幅,它正在将输出振幅实际上从450mV降低到225mV。

    因此,衰减器不会导致振幅级别问题。

    选中“Disable Remote EDID load”(禁用远程EDID加载)后,序列化程序中的某些配置会发生更改。

    谢谢!

    Selva S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    感谢您提供有用的信息。 我将详细了解所有禁用远程EDID加载的功能及其对利润的影响等  

    我们可以后退一步,您到底在做什么? 添加6dB的衰减/损耗并查看链路是否仍然工作?  

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    当然,在电缆中增加6dB损耗,并确保链路正常工作或不工作。

    因为同轴配置中有947串行化器和948解串行化器。 它在12dB以上工作,没有任何问题。  

    但是,949序列化器和948解串行化器组合在6dB的设置下不工作。

    现在我有唯一的信息, 在 949串行器和948解串器的组合中,禁用远程EDID使链接比6dB更好。  

    谢谢!

    Selva S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Selva,  

    在默认情况下,949是否与同轴电缆或双绞线绑定? 我正在检查,但我非常怀疑禁用远程EDID会影响同轴电缆/STP绑定模式。 您是否可以在检查/取消检查时捕获I2C日志以查看其是否发生变化?  

    我想知道当它等待远程EDID初始化而不报告锁定时,这是否会中断反信道/I2C通信。 您能否同时提供DES reg转储以查看它是否显示为已锁定?  

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    在默认情况下,949是否与同轴电缆或双绞线绑定? 我正在检查,但我非常怀疑禁用远程EDID会影响同轴电缆/STP绑定模式。 您是否可以在检查/取消检查时捕获I2C日志以查看其是否发生变化?  

    默认模式为同轴:请参阅对齐

    已发布带有/不带禁用EDID寄存器转储的串行器端。 (检查/取消检查)

    我想知道当它等待远程EDID初始化而不报告锁定时,这是否会中断反信道/I2C通信。

    是的,我也是这样想的。 我想这只是在发生。

    您能否同时提供DES reg转储以查看它是否已锁定?  

     我可以在锁定条件下共享DES reg转储。 让我检查一下。  

    谢谢!

    Selva s

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    我想,一旦您观察到DES侧注册,您会发现它实际上在两种情况下都锁定。 我还不清楚为什么有时它会报告为非同轴模式。 您是否可以根据EDID禁用复选框的状态检查这是否完全确定?

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    我有一个简短的问题,在evkit中,在10dB衰减后,您是否能够与反序列化器连接? 在同轴模式下,您是否有任何测试数据?

    是否可以在evkit上执行?

    我们可以轻松地进行交叉检查。  

    谢谢!

    塞尔瓦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    我的理解是在6dB后的反向通道受影响,因此EDID检查功能通过错误状态。由于该错误状态,像素时钟不会由串行器释放。

    如果我们禁用了EDID,则解串器和CDR锁定接收的像素时钟将发生,即使其大小为6dB或更高。

    然后正在进行初始化。 请与evkit核对,并确认是否相同?

    注意:禁用EDID也会影响到STP的同轴位。

    我不知道为什么会发生这种情况,

    在947中,串行器没有这种检查,因此它对我们的作用超过12dB衰减,没有任何问题。

    谢谢!

    塞尔瓦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    您是否有一个逻辑分析器来探测I2C总线以查看在禁用EDID复选框操作期间实际写入的寄存器? 如果直接写入同轴电缆/STP模式寄存器作为该复选框的影响,我会感到非常惊讶。  

    最终,我认为整个6dB调查与此复选框没有真正的关联。 例如,尝试移除6dB衰减...复选框是否仍会影响ALP中锁定/识别DES的能力?

    长而短,请保持选中远程EDID加载,因为您的应用程序中未使用此功能。

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢洛根

    我会尝试获取总线数据。 同时,请您也检查一下您的情况吗?

    谢谢!

    塞尔瓦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    我将检查我这边的寄存器预设,看看同轴电缆与STP问题是否可以复制。  

    此致  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请在EDID禁用和启用条件期间查找序列化器和反序列化器活动,Excel包含序列化器总线活动。 串行器地址0Ce2e.ti.com/.../949ser_5F00_no_5F00_edid_5F00_disable.txte2e.ti.com/.../949ser_5F00_edid_5F00_disable.txte2e.ti.com/.../948des_5F00_edid_5F00_disable.txte2e.ti.com/.../948des_5F00_no_5F00_edid_5F00_disable.txt

    e2e.ti.com/.../949_5F00_register_5F00_dump.xlsx

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Selva,  

    感谢您提供信息。  

    是的,在这两种情况下,使用948成功锁定,因此锁定状态不受此复选框的影响。 或者我错过了什么? 这些测试是否没有6dB衰减?

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    这些都经过测试,没有衰减。 锁定状态正常。 您是否检查了从同轴电缆更改为STP的配置。 我也会以6dB衰减进行开机自检。

    谢谢!

    塞尔瓦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    我看到现在的情况...从较高的层面来看,您看到不同利润结果的原因在于同轴电缆与STP模式。  

    它与EDID强制本身的选择无关,但当您点击"应用设置"时,所发生的情况是该选项卡中的其他设置将覆盖同轴带选择。 一天结束时,您只需将该部件固定到正确的模式,或直接使用寄存器更新设置。  

    即使您未取消选中"Disable remote EDID"(禁用远程EDID),也按"Apply settings"(应用设置)时,同轴电缆模式仍将更改为STP模式。

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    e2e.ti.com/.../2185.Register_5F00_dump_5F00_comparision.xlsx

    您好,Logan,  

    感谢您努力从日志中查找此信息。 因此,与同轴电缆相比,我对STP模式的理解使链路的利润更好?

    那么,让链路变得更好的原因是什么? 如您所知,与同轴模式相比,振幅也较小。  您还有其他建议或想法吗?

    寄存器转储比较显示,21个寄存器由于“应用设置”而受到影响,因此哪一个寄存器使我的链接更好。 我不确定仅STP就能改善我的链路。

    您能否进行交叉核对?

    解串器Reg比较:8个寄存器在解串器端受到影响

    谢谢

    Selva S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Selva,  

    我402.9708万我不确定STP是否会使我的链接更好。

    您是否可以使用带式配置修改同轴电缆与STP模式设置,以查看它是否影响链路边界?  

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    将带式电阻器更改为STP后,链路预算高达12dB,但由于一侧STP和另一侧同轴电缆配置,无法显示。 请参阅所连接的配置。


    e2e.ti.com/.../949ser_5F00_STP_5F00_12db_5F00_edid_5F00_disable.txte2e.ti.com/.../949ser_5F00_STP_5F00_12db_5F00_no_5F00_edid_5F00_disable.txte2e.ti.com/.../948des_5F00_STP-_5F00_12db_5F00_edid_5F00_disable.txte2e.ti.com/.../948des_5F00_STP_5F00_12db_5F00_no_5F00_edid_5F00_disable.txt

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Selva,  

    只是为了确保我仍在同一页上,您说STP模式比默认同轴模式改善了边距。 这是否正确? 在上述测试中,是否仅更改了腕带设置,或者您是否也在执行"应用设置"写入以更新其他值?  

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    1.我将其配置为STP模式。 链路在不使用"应用设置"的情况下工作至12dB。

    2.我在STP模式下再次尝试了“应用设置”,在将绑定配置为STP后,链路边界没有影响。

    3.在“应用设置”中,对其他寄存器有一些影响,但链接余量仍然良好。

    4.因此,两个日志文件都是附加的,供您参考。

    谢谢!

    塞尔瓦  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    如上所述,这在某种程度上是预料之中的。 同轴电缆模式与STP模式将具有不同的驱动器级别/振幅,并可能影响整体链路余量,尤其是当您人为地降低链路余量时,会出现12dB的下降。

    将402.2039万将输出振幅实际上从450mV降低到225mV。

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    我们有文档“传输通道要求和PCB/同轴电缆预算”,它显示同轴电缆可在1.84Ghz下工作 ,插入损耗大于12 dB的S21。  

    那么,让我知道如何使用  evkit测试12dB插入损耗余量?  

    谢谢!

    Selva S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    您是否可以附上您所指的文档?  

    为什么选择6dB来验证12 dB处的EVM? 需要考虑全通道插入损耗,因此链路的其余部分(电缆,印刷电路板,连接器等)将在链路上产生额外的dB插入损耗。  

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Logan,

    我正在澄清我的意见,以便更好地理解。

    949和947在印刷电路板中具有相同的插入损耗和返回损耗。  

    电缆损耗可忽略不计。  

    除PCB损耗和电缆损耗外,电缆外部添加的947至948链路最大为12dB。

    949和948链路最多只存在6 dB。 我们最初尝试使用12dB,但链路未建立。  
    我们慢慢地降低了该值,我们看到墨水连接小于或等于6dB


    这里的问题是这两个都在同轴电缆中,为什么与949的链路的利润较小?

    谢谢!

    塞尔瓦

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    </s>403.7873万

    IL/RL预算:  

    我们测量了IL / RL电缆+板+解串器侧,它也在限制范围内。

    [/引述]

    请提供电缆/板/印刷电路板的完整插入/返回损耗结果(带有或不带有增加的6dB损耗)。 我们的信道规格不是简单的"12db",而是实际取决于频率。 如果您不是以全1.84GHz运行,则其电缆预算将低于-12dB (例如-8.5dB @ 1.00GHz)。

    如果您提供了I/R损耗数据,我们可以将其与信道要求进行比较。

    此致,  

    Logan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Logan  

    请找到949和948的IL /RL。 从串行器端的交流电压盖到反串行器端的交流电压盖,包括印刷电路板跟踪/连接器/电缆等  

    S11 / S22 DOUT 0- 串行器(SMA -盖垫-跟踪->连接器)-同轴->(连接器-跟踪-盖垫- SMA)解串器
    频率 5MHz 10MHz 20MHz 100MHz 500MHz 1GHz 1.5GHz 1.84GHz
    测量值-串行器- S11 -16.23 -17.7 -20.69 -25.7 -23.55 -11.76 -13.5 -13.6
    测量值为-解串器- S22 -17.505 -18.8 -23.5 -30.1 -25.84 -12.75 -24.5 -16.99
    Dout 1 - 串行器(SMA -盖垫-跟踪->连接器)-同轴电缆->(连接器-跟踪-盖垫- SMA)解串器
    频率 5MHz 10MHz 20MHz 100MHz 500MHz 1GHz 1.5GHz 1.84GHz
    测量值-串行器- S11 -16.1 -17.55 -20.69 -25.9 -30.1 -11.43 -15.62 -10.2
    测量值为-解串器- S22 -17.32 -18.58 -23.66 -29.23 -22.82 -11.59 -23.6 -10.78
    Dout 0- 串行器(SMA -盖垫-跟踪->连接器)-同轴->(连接器-跟踪-盖垫- SMA)解串器
    频率 5MHz 10MHz 20MHz 100MHz 500MHz 1GHz 1.5GHz 1.84GHz
    测量位置-串行器至解串器 - S12 -0.0618 -0.108 -0.214 -0.689 -1.806 -3.063 -4.22 -5.089
    Dout 1 - 串行器(SMA -盖垫-跟踪->连接器)-同轴电缆->(连接器-跟踪-盖垫- SMA)解串器
    频率 5MHz 10MHz 20MHz 100MHz 500MHz 1GHz 1.5GHz 1.84GHz
    测量值为-串行器至解串器-S12 -0.06 -0.118 -0.233 -0.731 -0.183 -3.268 -4.13 -5.594

    插入损耗< 6dB。 回波损耗几乎相似。 我没有发现任何偏离要求的情况。  

    谢谢!

    Selva S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Selva,  

    您还需要获取 包含6dB的数据,以了解总损失是什么(可能它影响的程度超过附加适配器/连接器等仅影响6dB),因为这是您看到问题的地方。

    此外,如前所述,12dB实际上仅在1.8GHz时,在较低频率时会更低。 例如,1GHz需要-8.5dB (仅电缆)。 总之,当您添加6dB损耗时,可能违反了同轴特定信道规范(低于STP模式)。 如果在947/949之间有不同的结果,则可能是特定于设备的差异,正如Casey在另一线程中指出的那样。

    我们的完整渠道规范仅限于NDA,我建议联系您当地的FAE,他们可以帮助您访问该信息。  

    此致,  

    Logan