This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TS3USB3031:TS3USB3031能否用作3.1 1代解决方案

Guru**** 2976770 points

Other Parts Discussed in Thread: TS3USB3031, HD3SS460, HD3SS3212

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/576999/ts3usb3031-can-the-ts3usb3031-be-used-as-a-usb3-1-gen-1-solution

部件号:TS3USB3031
主题中讨论的其他部件: HD3SS460, HD3SS3212

TS3USB3031数据表显示6.5 GHz的3 dB带宽,但部件数据表仅表示它适合2.0。  它是否也可用于3.1 的第1代信令?

 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    请考虑HD3SS3212或HD3SS460。我们尚未为TS3USB3031 Gen 1描述其特征。我们将进行查看。