This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS16EV5110A:连接以太网电缆与交流耦合输入

Guru**** 2847390 points

Other Parts Discussed in Thread: DS16EV5110A, DS15BA101, DS16EV5110

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/602005/ds16ev5110a-interfacing-ethernet-cable-with-ac-coupled-input

部件号:DS16EV5110A
主题中讨论的其他部件: DS15BA101DS16EV5110

您好:

  我们需要通过100米以太网电缆传输4个通道250Mbps数据,需要在信号链中使用交流耦合。

  发射器是DS15BA101,接收器是DS16EV5110A,到目前为止,我们可以恢复125MHz时钟,但如果我们使用PRBS-7数据,那么我们只能达到62.5Mbps,您似乎拥有一个评估板 DS16EV51-AEVKC, 它可以在80米以上的CAT5 UTP上支持225Mbps,我有以下问题:

   1:DS16EV5110和DS16EV5110A之间有何区别?

   2:交流耦合接口是否会降低均衡器性能?

   3:对于输入接口, 50欧姆单阻抗控制和100欧姆差分阻抗控制之间是否存在差异 ?

   非常感谢您的帮助。

    此致!

    宜凡