This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PCA9306:如果PCA9306可以支持热插拔

Guru**** 2561390 points
Other Parts Discussed in Thread: PCA9306

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/635843/pca9306-if-pca9306-can-support-hot-plug

部件号:PCA9306

大家好,

我们的PCA9306设备是否支持热插拔应用?   谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    嗨Lilian,

    对于PCA9306,最好将下拉电阻器连接到EN引脚,然后将GPIO引脚从MCU/FPGA/MASTER连接到EN。 这样,PCA9306将被关闭,直到主控制器重新启用它。

    我还建议GPIO电压大于或至少等于两个电压(VreF1或Vref2)中的最低电压。

    谢谢!

    -Bobby