请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TUSB8041 工具/软件:Linux
尊敬的先生
您能告诉我为什么需要R1=90.9K_R2=10K_R2...... 1 % 1 %
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Linux
尊敬的先生
您能告诉我为什么需要R1=90.9K_R2=10K_R2...... 1 % 1 %