This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS250DF810EVM:DS250DF810

Guru**** 2763595 points

Other Parts Discussed in Thread: DS250DF810

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/640502/ds250df810evm-ds250df810

部件号:DS250DF810EVM
主题中讨论的其他部件:DS250DF810

是否可以使用上述EVM驱动具有以下标准的LVDS脉冲信号?

VCM:0.4V–1V

电压差:150mV–800mV

脉冲宽度:0.7ns–3ns

Trise/Tfall:20ps–500ps

脉冲周期:最小10ns