This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS6.5982万:TPS6.5982万和TPS6.5986万配置工具问题

Guru**** 2480055 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/568475/tps65982-tps65982-and-tps65986-configuration-tool-question

部件号:TPS6.5982万

您好,先生,

1.我可以知道TPS6.5982万配置工具与1.3 和2.1 版本的区别吗?
由于我们已安装测试配置工具,用于将电源传输20V/3A至戴尔XPS15和Mac Pro (15英寸)的2.1 构建固件发生过电流问题。
但是测试配置工具1.3 与 戴尔XPS15&Mac Pro (15英寸)功能建立相同的固件。

另一个问题是最终客户反馈在此情况下,我的TPS6.5986万没有问题。
2.我可以知道TPS6.5982万和TPS6.5986万配置工具的区别吗?