This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/DP8.364万T-EVK:USB连接

Guru**** 2468610 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/586406/ccs-dp83640t-evk-usb-connection

部件号:DP8.364万T-EVK
主题中讨论的其他部件:DP8.364万

工具/软件:Code Composer Studio

您好,  

我有一个DP8.364万评估板,一直在尝试使用National半导体模拟发射台程序通过USB端口连接到phy。 我下载了驱动程序并尝试在多台计算机上进行连接,但运气不佳。

我们一直在尝试ping PIC32以太网入门套件II (通过铜缆以太网) 通过拆除LAN8740 PHY子板 和PIC32以太网入门套件与dp8.364万评估板之间的运行跳线。我们已通读数据表中所有适当的卷线,但当我们尝试从我们的windows 7连接到dp8.364万评估板时, 我们无法连接。我们还在3个相同的PHY评估板上尝试了此操作。  

请告知:

WES