请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TUSB9261 我正在设计一种嵌入式设计,除了在USB集线器之前,在USB到SATA的任何地方都不使用5V电压。 我是否可以使用不同的分压器值,例如连接到3.3V的56.2k和10k来为VBUS提供所需的电压参考?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我正在设计一种嵌入式设计,除了在USB集线器之前,在USB到SATA的任何地方都不使用5V电压。 我是否可以使用不同的分压器值,例如连接到3.3V的56.2k和10k来为VBUS提供所需的电压参考?
谢谢