请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TUSB320 您好,
我在DRP模式下使用TUSB320来解决问题。
问题是:插入电源或设备后,CSR寄存器0x09 [7:6] Attached_State保持读数为00。
但是,当我使用演示板TUSB320 EVM RevB时, CSR寄存器0x09 [7:6] Attached_State可以快速更新值。
下面附上我的示意图。
我希望有人能给我一些短语
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.