请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:SN65DSI83 大家好,团队
我对SN65DSI83的VDSI_PIN范围有疑问。
我是否必须保持在推荐操作条件中指定的VDSI_PIN范围内?
峰值噪声叠加在LP模式的低电压上,该电压低于建议操作条件中指定的VDSI_PIN的下限。
除噪声外,该值高于-50mV。
此噪音可能是由REF_CLK上的串扰引起的。
此致,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.