This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN65DSI83:需要为网桥配置Linux驱动程序和Dtsi

Guru**** 2551110 points
Other Parts Discussed in Thread: SN65DSI83

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1096128/sn65dsi83-need-linux-driver-and-dtsi-configurations-for-the-bridge

部件号:SN65DSI83

大家好,

我们的定制主板基于IMX8MM + SN65DSI83桥接器,带10.1 英寸LVDS显示器。  

我有以下疑问,请您帮忙回答。  

1.在我们的设计中,i.MX8MM ==>MIPI-DSI ==>SN65DSI83 (LVDS桥接器)==>显示面板

2.在SN66DSI83上,其I2C SDA和SCL线路连接到测试点,ADDR接地,EN连接到IMX8MM。 此网桥是否可能仅将MIPI DSI输出发送到显示面板而不带I2C线路?  

3.如果是,请您帮助我们解决此问题。  

谢谢!

Raghavendra