This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TUSB4020BI:我是否可以使用FPGA 1.2V IO + 1/2电阻分压器来驱动此VBUS引脚?

Guru**** 2538930 points
Other Parts Discussed in Thread: TUSB4020BI

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1095264/tusb4020bi-can-i-use-fpga-1-2v-io-1-2-resistor-divider-to-drive-this-vbus-pin

部件号:TUSB4020BI

我的主板上没有5V和3.3V电压。 我是否可以使用FPGA 1.2V IO + 1/2电阻分压器(如50K,50k)来驱动此VBUS引脚?  

最终电压将约为0.6V,这与DS中建议的5V/10=0.5V非常相似。

此外,为什么DS为该VBUS引脚显示500mA? 我认为VBUS通常只吸引情侣。谢谢