This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [FAQ] DS90UB933-Q1:DS90UB933-Q1和DS90UB913A-Q1模式解码

Guru**** 2813875 points

Other Parts Discussed in Thread: DS90UB913A-Q1, DS90UB933-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1094850/faq-ds90ub933-q1-ds90ub933-q1-and-ds90ub913a-q1-mode-decode

部件号:DS90UB933-Q1
主题中讨论的其他部件:DS90UB913A-Q1

如何确定DS90UB933-Q1或DS90UB913A-Q1设备是否通过寄存器在RAW10,RAW12LF或RAW12HF下运行?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    远程反序列化器设置的操作模式可以通过寄存器0x05读回。 解码表如下所示:

    RAW10 RAW12LF RAW12HF
    0x05 = 0x14 0x05 = 0x10 0x05 = 0x18