This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DP8.3848万J:从PHY到RJ45的建议最大迹线长度

Guru**** 2927270 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1097790/dp83848j-recommended-maximum-trace-length-from-phy-to-rj45

部件号:DP8.3848万J

团队成员:

 我的客户使用DP8.3848万 PHY,但他们对PCB布局有一些限制,因此他们想确认PHY到RJ45侧的最大迹线长度

 同时,建议在从规格检查后,将MAC连接到PHY的长度小于2英寸。