如果发射振幅超过最大振幅0.88Vp-p @额态模式和0.44Vp-p @分离模式,会发生什么情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好Nasser:
我正在与撒哈拉合作,这里有一些相关的问题。
1.我们关注输入信号电平"VSDI_IO_launch "是否超出您建议的操作条件,不像ESD Serge,而是面对高电平发射器。
以下假设是否正确?
-如果输入电压在ABS最大额定值- 0.5 至2.75 V范围内,则可靠性不是问题。
-前端电路可能饱和,然后减少眼部开度。
2. 为了更精确地预期前端放大器的功能,我们想知道正常模式和分流模式的-6dB控制电路结构。 哪个是正确的图像?
- NFB环路增益更改为降低-6dB增益。
前端添加了-6dB的衬垫衰减器。
此致,
Mochizuki