Other Parts Discussed in Thread: TUSB9261
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TUSB9261 大家好,
TUSB9261可以使用25MHz 晶体吗?我看到大多数使用40M晶体,但 我的客户不能使用40M晶体吗?
第二个问题是:此部件是否必须为SPI提供闪存? 如果是,闪存的要求是什么?
非常感谢。
顺祝商祺!Sunny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.