This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS90UB941AS-Q1:是 DS90UB941AS-Q1 MIPI D-PHY v1.2/DSI v1.3.1、可集成到仅具有 MIPI D-PHY 1.2和 DSI v1.1的处理器

Guru**** 2546020 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1124540/ds90ub941as-q1-is-the-ds90ub941as-q1-mipi-d-phy-v1-2-dsi-v1-3-1-compartible-to-a-processor-that-only-have-mipi-d-phy-1-2-and-dsi-v1-1

器件型号:DS90UB941AS-Q1

大家好、

我们尝试将 DS90UB941xxx 与仅支持 MIPI D-PHY v1.2和 DSI v1.1的处理器连接。

这会是个问题吗? 我们是否必须配置941?

 此致、

Ulrich