This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DP83826I:CAN#39;t link to chip from PC (or Hub)(从 PC (或集线器)到芯片)

Guru**** 2550780 points
Other Parts Discussed in Thread: DP83826I

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1121580/dp83826i-can-t-link-to-chip-from-pc-or-hub

器件型号:DP83826I

 在将 DP83826I 芯片连接到 PC 时遇到重大问题(涉及集线器并直接尝试)。  

使用 STMCube 生成的 LWIP 协议栈(STM32)。

示波器上测量的1-RCV_CLK 时钟为25MHz

2-我们认为通过示波器探针在 MDI 引脚上有 FLP 活动。

3-状态寄存器位显示未链接。

4-原理图已附。

5-REGSe2e.ti.com/.../3175.V86652_5F00_3.3.pdf

寄存器地址00值= 1000
寄存器地址01值= 786D
寄存器地址02值= 2000
寄存器地址03值= A130
寄存器地址04值= 1E1
寄存器地址05值= 45E1
寄存器地址06值= 7
寄存器地址07值= 2001
寄存器地址08值= 0
寄存器地址09值= 0
寄存器地址0A 值= 1000
寄存器地址0b 值= 0
寄存器地址0C 值= 0
寄存器地址0D 值= 0
寄存器地址0E 值= 0
寄存器地址0F 值= 0
寄存器地址10值= 215
寄存器地址11值= 108
寄存器地址12值= 6400
寄存器地址13值= 2800
寄存器地址14值= 0
寄存器地址15值= 0
寄存器地址16值= 100
寄存器地址17值= 41
寄存器地址18值= 0
寄存器地址19值= CC01
寄存器地址1A 值= 0
寄存器地址1B 值= 7D
寄存器地址1C 值= 424
寄存器地址1D 值= 0
寄存器地址1E 值= 102
寄存器地址1F 值= 0