This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TCA9535:3.3V VDD 的 VOH 电平说明

Guru**** 2949900 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1058694/tca9535-clarification-on-voh-level-for-3-3-vdd

器件型号:TCA9535

VDD- 3.3V

-我们将所有 IO 端口用作输出引脚,拉电流为0.3mA

-在数据表第5页、仅提到 VOH min  

-对于源电流0.3mA、VOH 最小值典型值和最大值是多少  

——请同时提及最坏情况