This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS125DF410:TX CDR 未锁定

Guru**** 2387360 points
Other Parts Discussed in Thread: DS125DF410
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1117292/ds125df410-tx-cdr-not-locking

器件型号:DS125DF410
尊敬的 TI 团队:
我们将 DS125DF410重定时器用于以太网插件卡、然后通过 SFP+电缆连接到链路伙伴 RX CDR 处于锁定状态、但 TX CDR 未锁定。 但我们进行了 SFI TX 合规性测试、SoC 生成了 PRBS 9和 PRBS 31模式、并通过重定时输出发送该模式、并捕获了良好的眼图。 如果我们缺少任何设置、我们将分享您的反馈。
0x0	Shared Registers_0x00	00
0x1	Shared Registers_0x01	D1
0x2	Shared Registers_0x02	00
0x3	Shared Registers_0x03	00
0x4	Shared Registers_0x04	01
0x5	Shared Registers_0x05	10
0x6	Shared Registers_0x06	00
0x7	Shared Registers_0x07	04
0xFF	Global Registers_0xFF	00
0x0	Channel 0_0x00	00
0x1	Channel 0_0x01	00
0x2	Channel 0_0x02	04
0x3	Channel 0_0x03	A5
0x4	Channel 0_0x04	00
0x5	Channel 0_0x05	00
0x6	Channel 0_0x06	00
0x7	Channel 0_0x07	00
0x8	Channel 0_0x08	00
0x9	Channel 0_0x09	00
0xA	Channel 0_0x0A	10
0xB	Channel 0_0x0B	0F
0xC	Channel 0_0x0C	08
0xD	Channel 0_0x0D	00
0xE	Channel 0_0x0E	93
0xF	Channel 0_0x0F	69
0x10	Channel 0_0x10	3A
0x11	Channel 0_0x11	E0
0x12	Channel 0_0x12	A0
0x13	Channel 0_0x13	30
0x14	Channel 0_0x14	00
0x15	Channel 0_0x15	52
0x16	Channel 0_0x16	7A
0x17	Channel 0_0x17	36
0x18	Channel 0_0x18	40
0x19	Channel 0_0x19	23
0x1A	Channel 0_0x1A	00
0x1B	Channel 0_0x1B	03
0x1C	Channel 0_0x1C	24
0x1D	Channel 0_0x1D	00
0x1E	Channel 0_0x1E	21
0x1F	Channel 0_0x1F	55
0x20	Channel 0_0x20	00
0x21	Channel 0_0x21	00
0x22	Channel 0_0x22	00
0x23	Channel 0_0x23	C0
0x24	Channel 0_0x24	40
0x25	Channel 0_0x25	00
0x26	Channel 0_0x26	00
0x27	Channel 0_0x27	00
0x28	Channel 0_0x28	00
0x29	Channel 0_0x29	00
0x2A	Channel 0_0x2A	30
0x2B	Channel 0_0x2B	00
0x2C	Channel 0_0x2C	72
0x2D	Channel 0_0x2D	82
0x2E	Channel 0_0x2E	00
0x2F	Channel 0_0x2F	F6
0x30	Channel 0_0x30	00
0x31	Channel 0_0x31	40
0x32	Channel 0_0x32	11
0x33	Channel 0_0x33	88
0x34	Channel 0_0x34	BF
0x35	Channel 0_0x35	1F
0x36	Channel 0_0x36	31
0x37	Channel 0_0x37	00
0x38	Channel 0_0x38	00
0x39	Channel 0_0x39	00
0x3A	Channel 0_0x3A	A5
0x3B	Channel 0_0x3B	00
0x3C	Channel 0_0x3C	00
0x3D	Channel 0_0x3D	00
0x3E	Channel 0_0x3E	80
0x3F	Channel 0_0x3F	00
0x40	Channel 0_0x40	00
0x41	Channel 0_0x41	01
0x42	Channel 0_0x42	04
0x43	Channel 0_0x43	10
0x44	Channel 0_0x44	40
0x45	Channel 0_0x45	08
0x46	Channel 0_0x46	02
0x47	Channel 0_0x47	80
0x48	Channel 0_0x48	03
0x49	Channel 0_0x49	0C
0x4A	Channel 0_0x4A	30
0x4B	Channel 0_0x4B	41
0x4C	Channel 0_0x4C	50
0x4D	Channel 0_0x4D	C0
0x4E	Channel 0_0x4E	60
0x4F	Channel 0_0x4F	90
0x50	Channel 0_0x50	88
0x51	Channel 0_0x51	82
0x52	Channel 0_0x52	A0
0x53	Channel 0_0x53	46
0x54	Channel 0_0x54	52
0x55	Channel 0_0x55	8C
0x56	Channel 0_0x56	B0
0x57	Channel 0_0x57	C8
0x58	Channel 0_0x58	57
0x59	Channel 0_0x59	5D
0x5A	Channel 0_0x5A	69
0x5B	Channel 0_0x5B	75
0x5C	Channel 0_0x5C	D5
0x5D	Channel 0_0x5D	99
0x5E	Channel 0_0x5E	96
0x5F	Channel 0_0x5F	A5
0x60	Channel 0_0x60	00
0x61	Channel 0_0x61	00
0x62	Channel 0_0x62	00
0x63	Channel 0_0x63	00
0x64	Channel 0_0x64	00
0x65	Channel 0_0x65	00
0x66	Channel 0_0x66	00
0x67	Channel 0_0x67	20
0x68	Channel 0_0x68	00
0x69	Channel 0_0x69	0A
0x6A	Channel 0_0x6A	44
0x6B	Channel 0_0x6B	00
0x6C	Channel 0_0x6C	00
0x6D	Channel 0_0x6D	00
0x6E	Channel 0_0x6E	00
0x6F	Channel 0_0x6F	00
0x70	Channel 0_0x70	03
0x71	Channel 0_0x71	20
0x72	Channel 0_0x72	00
0x73	Channel 0_0x73	00
0x74	Channel 0_0x74	00
0x75	Channel 0_0x75	00
0x0	Channel 1_0x00	00
0x1	Channel 1_0x01	00
0x2	Channel 1_0x02	00
0x3	Channel 1_0x03	A5
0x4	Channel 1_0x04	00
0x5	Channel 1_0x05	00
0x6	Channel 1_0x06	00
0x7	Channel 1_0x07	00
0x8	Channel 1_0x08	00
0x9	Channel 1_0x09	00
0xA	Channel 1_0x0A	10
0xB	Channel 1_0x0B	0F
0xC	Channel 1_0x0C	08
0xD	Channel 1_0x0D	00
0xE	Channel 1_0x0E	93
0xF	Channel 1_0x0F	69
0x10	Channel 1_0x10	3A
0x11	Channel 1_0x11	E0
0x12	Channel 1_0x12	A0
0x13	Channel 1_0x13	30
0x14	Channel 1_0x14	00
0x15	Channel 1_0x15	52
0x16	Channel 1_0x16	7A
0x17	Channel 1_0x17	36
0x18	Channel 1_0x18	40
0x19	Channel 1_0x19	23
0x1A	Channel 1_0x1A	00
0x1B	Channel 1_0x1B	03
0x1C	Channel 1_0x1C	24
0x1D	Channel 1_0x1D	00
0x1E	Channel 1_0x1E	21
0x1F	Channel 1_0x1F	55
0x20	Channel 1_0x20	00
0x21	Channel 1_0x21	00
0x22	Channel 1_0x22	00
0x23	Channel 1_0x23	C0
0x24	Channel 1_0x24	44
0x25	Channel 1_0x25	00
0x26	Channel 1_0x26	00
0x27	Channel 1_0x27	00
0x28	Channel 1_0x28	00
0x29	Channel 1_0x29	00
0x2A	Channel 1_0x2A	30
0x2B	Channel 1_0x2B	00
0x2C	Channel 1_0x2C	72
0x2D	Channel 1_0x2D	82
0x2E	Channel 1_0x2E	00
0x2F	Channel 1_0x2F	F6
0x30	Channel 1_0x30	00
0x31	Channel 1_0x31	40
0x32	Channel 1_0x32	11
0x33	Channel 1_0x33	88
0x34	Channel 1_0x34	BF
0x35	Channel 1_0x35	1F
0x36	Channel 1_0x36	31
0x37	Channel 1_0x37	00
0x38	Channel 1_0x38	00
0x39	Channel 1_0x39	00
0x3A	Channel 1_0x3A	A5
0x3B	Channel 1_0x3B	00
0x3C	Channel 1_0x3C	00
0x3D	Channel 1_0x3D	00
0x3E	Channel 1_0x3E	80
0x3F	Channel 1_0x3F	00
0x40	Channel 1_0x40	00
0x41	Channel 1_0x41	01
0x42	Channel 1_0x42	04
0x43	Channel 1_0x43	10
0x44	Channel 1_0x44	40
0x45	Channel 1_0x45	08
0x46	Channel 1_0x46	02
0x47	Channel 1_0x47	80
0x48	Channel 1_0x48	03
0x49	Channel 1_0x49	0C
0x4A	Channel 1_0x4A	30
0x4B	Channel 1_0x4B	41
0x4C	Channel 1_0x4C	50
0x4D	Channel 1_0x4D	C0
0x4E	Channel 1_0x4E	60
0x4F	Channel 1_0x4F	90
0x50	Channel 1_0x50	88
0x51	Channel 1_0x51	82
0x52	Channel 1_0x52	A0
0x53	Channel 1_0x53	46
0x54	Channel 1_0x54	52
0x55	Channel 1_0x55	8C
0x56	Channel 1_0x56	B0
0x57	Channel 1_0x57	C8
0x58	Channel 1_0x58	57
0x59	Channel 1_0x59	5D
0x5A	Channel 1_0x5A	69
0x5B	Channel 1_0x5B	75
0x5C	Channel 1_0x5C	D5
0x5D	Channel 1_0x5D	99
0x5E	Channel 1_0x5E	96
0x5F	Channel 1_0x5F	A5
0x60	Channel 1_0x60	00
0x61	Channel 1_0x61	00
0x62	Channel 1_0x62	00
0x63	Channel 1_0x63	00
0x64	Channel 1_0x64	00
0x65	Channel 1_0x65	00
0x66	Channel 1_0x66	00
0x67	Channel 1_0x67	20
0x68	Channel 1_0x68	00
0x69	Channel 1_0x69	0A
0x6A	Channel 1_0x6A	44
0x6B	Channel 1_0x6B	00
0x6C	Channel 1_0x6C	00
0x6D	Channel 1_0x6D	00
0x6E	Channel 1_0x6E	00
0x6F	Channel 1_0x6F	00
0x70	Channel 1_0x70	03
0x71	Channel 1_0x71	20
0x72	Channel 1_0x72	00
0x73	Channel 1_0x73	00
0x74	Channel 1_0x74	00
0x75	Channel 1_0x75	00
0x0	Channel 2_0x00	00
0x1	Channel 2_0x01	00
0x2	Channel 2_0x02	00
0x3	Channel 2_0x03	A5
0x4	Channel 2_0x04	00
0x5	Channel 2_0x05	00
0x6	Channel 2_0x06	00
0x7	Channel 2_0x07	00
0x8	Channel 2_0x08	00
0x9	Channel 2_0x09	00
0xA	Channel 2_0x0A	10
0xB	Channel 2_0x0B	0F
0xC	Channel 2_0x0C	08
0xD	Channel 2_0x0D	00
0xE	Channel 2_0x0E	93
0xF	Channel 2_0x0F	69
0x10	Channel 2_0x10	3A
0x11	Channel 2_0x11	E0
0x12	Channel 2_0x12	A0
0x13	Channel 2_0x13	30
0x14	Channel 2_0x14	00
0x15	Channel 2_0x15	52
0x16	Channel 2_0x16	7A
0x17	Channel 2_0x17	36
0x18	Channel 2_0x18	40
0x19	Channel 2_0x19	23
0x1A	Channel 2_0x1A	00
0x1B	Channel 2_0x1B	03
0x1C	Channel 2_0x1C	24
0x1D	Channel 2_0x1D	00
0x1E	Channel 2_0x1E	21
0x1F	Channel 2_0x1F	55
0x20	Channel 2_0x20	00
0x21	Channel 2_0x21	00
0x22	Channel 2_0x22	00
0x23	Channel 2_0x23	C0
0x24	Channel 2_0x24	44
0x25	Channel 2_0x25	00
0x26	Channel 2_0x26	00
0x27	Channel 2_0x27	00
0x28	Channel 2_0x28	00
0x29	Channel 2_0x29	00
0x2A	Channel 2_0x2A	30
0x2B	Channel 2_0x2B	00
0x2C	Channel 2_0x2C	72
0x2D	Channel 2_0x2D	82
0x2E	Channel 2_0x2E	00
0x2F	Channel 2_0x2F	F6
0x30	Channel 2_0x30	00
0x31	Channel 2_0x31	40
0x32	Channel 2_0x32	11
0x33	Channel 2_0x33	88
0x34	Channel 2_0x34	BF
0x35	Channel 2_0x35	1F
0x36	Channel 2_0x36	31
0x37	Channel 2_0x37	00
0x38	Channel 2_0x38	00
0x39	Channel 2_0x39	00
0x3A	Channel 2_0x3A	A5
0x3B	Channel 2_0x3B	00
0x3C	Channel 2_0x3C	00
0x3D	Channel 2_0x3D	00
0x3E	Channel 2_0x3E	80
0x3F	Channel 2_0x3F	00
0x40	Channel 2_0x40	00
0x41	Channel 2_0x41	01
0x42	Channel 2_0x42	04
0x43	Channel 2_0x43	10
0x44	Channel 2_0x44	40
0x45	Channel 2_0x45	08
0x46	Channel 2_0x46	02
0x47	Channel 2_0x47	80
0x48	Channel 2_0x48	03
0x49	Channel 2_0x49	0C
0x4A	Channel 2_0x4A	30
0x4B	Channel 2_0x4B	41
0x4C	Channel 2_0x4C	50
0x4D	Channel 2_0x4D	C0
0x4E	Channel 2_0x4E	60
0x4F	Channel 2_0x4F	90
0x50	Channel 2_0x50	88
0x51	Channel 2_0x51	82
0x52	Channel 2_0x52	A0
0x53	Channel 2_0x53	46
0x54	Channel 2_0x54	52
0x55	Channel 2_0x55	8C
0x56	Channel 2_0x56	B0
0x57	Channel 2_0x57	C8
0x58	Channel 2_0x58	57
0x59	Channel 2_0x59	5D
0x5A	Channel 2_0x5A	69
0x5B	Channel 2_0x5B	75
0x5C	Channel 2_0x5C	D5
0x5D	Channel 2_0x5D	99
0x5E	Channel 2_0x5E	96
0x5F	Channel 2_0x5F	A5
0x60	Channel 2_0x60	00
0x61	Channel 2_0x61	00
0x62	Channel 2_0x62	00
0x63	Channel 2_0x63	00
0x64	Channel 2_0x64	00
0x65	Channel 2_0x65	00
0x66	Channel 2_0x66	00
0x67	Channel 2_0x67	20
0x68	Channel 2_0x68	00
0x69	Channel 2_0x69	0A
0x6A	Channel 2_0x6A	44
0x6B	Channel 2_0x6B	00
0x6C	Channel 2_0x6C	00
0x6D	Channel 2_0x6D	00
0x6E	Channel 2_0x6E	00
0x6F	Channel 2_0x6F	00
0x70	Channel 2_0x70	03
0x71	Channel 2_0x71	20
0x72	Channel 2_0x72	00
0x73	Channel 2_0x73	00
0x74	Channel 2_0x74	00
0x75	Channel 2_0x75	00
0x0	Channel 3_0x00	00
0x1	Channel 3_0x01	00
0x2	Channel 3_0x02	04
0x3	Channel 3_0x03	57
0x4	Channel 3_0x04	00
0x5	Channel 3_0x05	00
0x6	Channel 3_0x06	00
0x7	Channel 3_0x07	00
0x8	Channel 3_0x08	00
0x9	Channel 3_0x09	00
0xA	Channel 3_0x0A	10
0xB	Channel 3_0x0B	0F
0xC	Channel 3_0x0C	08
0xD	Channel 3_0x0D	00
0xE	Channel 3_0x0E	93
0xF	Channel 3_0x0F	69
0x10	Channel 3_0x10	3A
0x11	Channel 3_0x11	E0
0x12	Channel 3_0x12	A0
0x13	Channel 3_0x13	30
0x14	Channel 3_0x14	00
0x15	Channel 3_0x15	52
0x16	Channel 3_0x16	7A
0x17	Channel 3_0x17	36
0x18	Channel 3_0x18	40
0x19	Channel 3_0x19	23
0x1A	Channel 3_0x1A	00
0x1B	Channel 3_0x1B	03
0x1C	Channel 3_0x1C	24
0x1D	Channel 3_0x1D	00
0x1E	Channel 3_0x1E	21
0x1F	Channel 3_0x1F	55
0x20	Channel 3_0x20	00
0x21	Channel 3_0x21	00
0x22	Channel 3_0x22	00
0x23	Channel 3_0x23	C0
0x24	Channel 3_0x24	44
0x25	Channel 3_0x25	00
0x26	Channel 3_0x26	00
0x27	Channel 3_0x27	00
0x28	Channel 3_0x28	00
0x29	Channel 3_0x29	00
0x2A	Channel 3_0x2A	30
0x2B	Channel 3_0x2B	00
0x2C	Channel 3_0x2C	72
0x2D	Channel 3_0x2D	82
0x2E	Channel 3_0x2E	00
0x2F	Channel 3_0x2F	F6
0x30	Channel 3_0x30	00
0x31	Channel 3_0x31	40
0x32	Channel 3_0x32	11
0x33	Channel 3_0x33	88
0x34	Channel 3_0x34	BF
0x35	Channel 3_0x35	1F
0x36	Channel 3_0x36	31
0x37	Channel 3_0x37	1D
0x38	Channel 3_0x38	00
0x39	Channel 3_0x39	00
0x3A	Channel 3_0x3A	A5
0x3B	Channel 3_0x3B	00
0x3C	Channel 3_0x3C	00
0x3D	Channel 3_0x3D	00
0x3E	Channel 3_0x3E	80
0x3F	Channel 3_0x3F	00
0x40	Channel 3_0x40	00
0x41	Channel 3_0x41	01
0x42	Channel 3_0x42	04
0x43	Channel 3_0x43	10
0x44	Channel 3_0x44	40
0x45	Channel 3_0x45	08
0x46	Channel 3_0x46	02
0x47	Channel 3_0x47	80
0x48	Channel 3_0x48	03
0x49	Channel 3_0x49	0C
0x4A	Channel 3_0x4A	30
0x4B	Channel 3_0x4B	41
0x4C	Channel 3_0x4C	50
0x4D	Channel 3_0x4D	C0
0x4E	Channel 3_0x4E	60
0x4F	Channel 3_0x4F	90
0x50	Channel 3_0x50	88
0x51	Channel 3_0x51	82
0x52	Channel 3_0x52	A0
0x53	Channel 3_0x53	46
0x54	Channel 3_0x54	52
0x55	Channel 3_0x55	8C
0x56	Channel 3_0x56	B0
0x57	Channel 3_0x57	C8
0x58	Channel 3_0x58	57
0x59	Channel 3_0x59	5D
0x5A	Channel 3_0x5A	69
0x5B	Channel 3_0x5B	75
0x5C	Channel 3_0x5C	D5
0x5D	Channel 3_0x5D	99
0x5E	Channel 3_0x5E	96
0x5F	Channel 3_0x5F	A5
0x60	Channel 3_0x60	00
0x61	Channel 3_0x61	00
0x62	Channel 3_0x62	00
0x63	Channel 3_0x63	00
0x64	Channel 3_0x64	00
0x65	Channel 3_0x65	00
0x66	Channel 3_0x66	00
0x67	Channel 3_0x67	20
0x68	Channel 3_0x68	00
0x69	Channel 3_0x69	0A
0x6A	Channel 3_0x6A	44
0x6B	Channel 3_0x6B	00
0x6C	Channel 3_0x6C	00
0x6D	Channel 3_0x6D	00
0x6E	Channel 3_0x6E	00
0x6F	Channel 3_0x6F	00
0x70	Channel 3_0x70	03
0x71	Channel 3_0x71	20
0x72	Channel 3_0x72	00
0x73	Channel 3_0x73	00
0x74	Channel 3_0x74	00
0x75	Channel 3_0x75	00
  
谢谢、
Sathish。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    有助于调试的两个问题:

    • 您能否澄清哪些重定时器通道(从0到3)是 Tx、哪些是 Rx?
    • 看起来您使用的是 TI SigCon Architect GUI。 重现问题后、您可以通过单击低级页面上的"Save config"来保存完整的重定时器寄存器值吗? 然后、您可以将保存的".cfg"文件发送给我

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 罗德里戈·纳塔尔、

    我们有两个 SFI 端口、端口0 CH0为 RX、CH1为 TX、端口1 CH2为 RX、CH3为 TX。

    e2e.ti.com/.../DS125DF410.cfg

    谢谢、

    Sathish。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,Sathish。

    我已查看您的寄存器日志文件。 我看到的主要观察结果如下:

    1. CTLE 似乎已收敛到默认 CTLE 表的升压值0xA5、最高升压设置。 这对于低损耗 SFI 通道没有意义。 不知怎么说、重定时器 Rx EQ 并不是自动优化的
    2. 对于任何通道、似乎都不符合 ppm 检查
    3. 某些通道未满足 SBT 检查

    请参阅下面的调试建议、

    • 如果强制 CTLE = 0x00、您是否能够看到重定时器通道获取 CDR 锁定? 请参阅以下说明

      表:强制 CTLE 升压值为0

       

       

      步骤

       

      共享/通道寄存器集

       

      操作

      寄存器地址[十六进制]

      寄存器值[十六进制]

      写入掩码[十六进制]

       

      注释

       

      1

       

      通道

       

      写入

       

      03

       

      00

       

      FF

      将 CTLE BOOST 设置为0x00

       

      2.

       

      通道

       

      写入

       

      3A

       

      00

       

      FF

      将 CTLE BOOST 设置为0x00。

       

       

      3.

       

      通道

       

      写入

       

      2D

       

      08

       

      08

      CTLE 覆盖启用

    • 如果您还通过设置通道寄存器0x0C[3]=0来禁用单位转换(SBT)检查、您是否看到 CDR 锁定?
    • 如果您还通过设置通道寄存器0x2F[2]= 0来禁用 PPM 检查、您是否看到 CDR 锁定?

     谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好 罗德里戈·纳塔尔
    我们按照以上说明操作、然后测试了 CDR 未锁定。

    我们计划测量重定时器的输入原始数据、连接差分有源探头、然后测试 CDR (端口0 CH1和 CH2)正在锁定。 因此、我们怀疑 SI 相关问题、并联系了内部 SI 团队。 他们说这与配置问题有关。  如果我们缺少活动探头的任何设置或影响、请分享您的反馈。


    谢谢、
    Sathish。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的更新。 我将此 E2E 帖子分类为"暂时关闭"、因为 TI 目前没有未完成的待处理开放操作。

    此致、

    罗德里戈

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我不确定这里还有什么要做的。 我已经查看了您的配置文件、但没有发现设置异常。 我唯一能推测的是重定时器输入信号过均衡的可能性。

    • 根据您的消息"我们使用 DS125DF410重定时器作为以太网插件卡、然后通过 SFP+电缆连接到链路伙伴 RX CDR 处于锁定状态、但 TX CDR 处于未锁定状态"
      • 问题:Tx CDR 未锁定的大致输入通道插入损耗是多少? 您能否提供代表性的 s 参数?
      • 问题:对于发送到此重定时器 Rx 通道但未获取 CDR 锁定的 SerDes、其 Tx 前标和后标设置是什么? 如果通道短路、TI 建议将前标和后标去加重设置为零

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好罗德里戈·纳塔尔、

    感谢您的回复。

    我们正在进行 SI 验证、将很快与您分享 S 参数。

    实际上、我们禁用了 TX 通道均衡、然后测量了10.312Gbps 数据速率并捕获了良好的眼图。

    我们的情况如下:

    如果没有连接伙伴、TX CDR 将锁定

    与链路合作伙伴一起、RX CDR 处于锁定状态、TX CDR 处于解锁状态

    与链路伙伴一起、我们在 TXP 和 TXN 中连接了差分有源探头、以检查传输数据、但 TX CDR 和 RX CDR 会锁定 CDR 并使 CDR 保持稳定。

    那么、是否有任何阻抗不匹配或寄生 电容会影响 CDR 锁定或  源探头的存在、它是否正常工作?

    谢谢、

    Sathish。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我不会期望阻抗不匹配问题会阻止 CDR 锁定。

    根据您的消息:如果没有链接伙伴,TX CDR 将锁定。 与链路合作伙伴一起、RX CDR 处于锁定状态、TX CDR 处于解锁状态

    • 问题:在这两种情况下、重定时器输入信号有何不同?

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的确认。

    我们还会对不同的行为感到惊讶、但使用有源探头可以正常工作。  因此、我请求您告诉我您的空闲情况、我将与 SI 团队建立一个电话联系。

    谢谢、
    Sathish。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果可能、我希望您在电话会议之前回答我的开放式问题:

    1. 系统中重定时器输入通道的 S 参数
    2. CDR 锁定与解锁情况下的重定时器输入信号特性说明(例如电压振幅差分、TX 均衡设置和抖动一致性)

    在我看来、使用有源探头观察到的结果更像是测量伪影。

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好罗德里戈·纳塔尔、

    我们正在与内部 SI 团队合作处理通道插入损耗和 s 参数、并在收到报告后共享报告。

    PFA 重定时器 CDR 锁定状态和眼图详细信息、供您参考。

    e2e.ti.com/.../DS125DF410SQ_5F00_Eye.pptx

    e2e.ti.com/.../Port-0_5F00_TX-eye_5F00_Retimer-Output.pdf

    谢谢、

    Sathish。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的更新。 我的一个主要评论是、您的重定时器输入眼图张开度监视器(EOM) 2D 图看起来非常不寻常。 在正常情况下、EOM 图应与下面的示例图类似。 在下图中、您有一个 CML 差分信号、该信号在-400至+400之间摆动、并以直流值0为中心。  

    您的图不像这样。 你看起来真的很奇怪。 我想推测系统板上的重定时器输入信号有一些探测信号。

    • 您能否确认您已在系统板上为 DS125DF410重定时器高速输入和输出实施了交流耦合电容器?
    • 重定时器的信号输入的 Tx 设置是什么?
      • 电压输出差分
      • TX 后标和前标去加重

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好罗德里戈·纳塔尔、


    以下是我的评论

    您能否确认您已在系统板上为 DS125DF410重定时器高速输入和输出实施了交流耦合电容器?
    答案:是的、我们在重定时器的输入和输出上有交流耦合电容器。

    重定时器的信号输入的 Tx 设置是什么?
    ANS:数据速率- 10.312Gb

    电压输出差分
    答案:1000mV

    TX 后标和前标去加重
    答案:去加重值为零。

    谢谢、
    Sathish。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢。 此时、我将等待您的通道 s 参数、并重新计时 CDR 锁定与非锁定情况下的通道寄存器日志(如果可能、完全寄存器转储)。

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好罗德里戈·纳塔尔、

    很抱歉耽误你的时间。

    我有压缩的 S 参数模型、带有一个较短的 ppt、可供您了解不同的模型可能与原理图中的不同部分相关。

    e2e.ti.com/.../TI_5F00_Collateral.zipe2e.ti.com/.../2185.DS125DF410.cfg

    谢谢、

    Sathish

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    • 根据您的".cfg"文件、活动通道(CH0和 CH3)显示 CDR 状态寄存器的值0x04。 这意味着不符合 PPM 检查、同时满足其他 CDR 锁定限定符
      • 建议:为了进行调试、通过设置通道寄存器0x2F[2]= 0来禁用重定时器 PPM 检查
    • 您的重定时器通道似乎具有低插入损耗
      • 建议:尝试强制使用 CTLE=0、最低 CTLE 升压设置。 请参阅下面的通道寄存器写入例程。

    寄存      器值   掩码    注释

    2D         08          08          //启用 CTLE 覆盖

    3A         00          FF          //强制 CTLE=0

    03          00          FF          //Force CTLE=0

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请提供与我的最新回复相关的反馈。 鉴于您报告的重定时器结果、我相信它提供了合适的调试路径。

    谢谢、

    罗德里戈

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好罗德里戈·纳塔尔、

    我们配置了上述建议、然后测试了 CDR 未锁定。 因此、我请求您告诉我您的空闲时间、我将设置一个 MS 团队呼叫。

    供参考、端口1 (CH2和 CH3)被旁路。

    e2e.ti.com/.../DS125DF410SQ.cfg

    谢谢、
    Sathish。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    根据您共享的最新 CFG 文件:

    • CH0和 CH2没有输入信号
    • CH1显示 CDR 锁定和良好的眼图张开值
    • CH3显示了 CTLE=0xA5时的零眼图张开值、这是最大 CTLE 升压。 考虑到您提供的通道详细信息、这不是最佳选择。 可能会发生过度均衡。
      • 请在此处应用我建议的 CTLE=0设置、然后在针对特定配置情况进行系统测试后共享您的重定时器寄存器日志结果。
      • 请再次参阅以下建议的 CTLE=0通道寄存器设置。

    寄存      器值   掩码    注释

    2D         08          08          //启用 CTLE 覆盖

    3A         00          FF          //强制 CTLE=0

    03          00          FF          //Force CTLE=0

    问题:您为什么绕过通道2和3?

    谢谢、

    罗德里戈

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    罗德里戈、您好!

    我们启用了 CH2和 CH3并配置了建议设置、然后测试的 CDR 未锁定。

    PFA SCH 方框图、平台上有 RX 路径上带电容的多路复用器、然后连接到 PCIe 连接器。 在多路复用器和重定时器之间添加卡、TX 路径上默认为0欧姆、RX 路径上默认为220nF。 将0欧姆电阻替换为 TX 路径上的220nF 后、CDR 会锁定且眼图良好。

    是否有任何建议将电容器放置在靠近重定时器的位置?   

    e2e.ti.com/.../BD_5F00_AIC1.pptx

    谢谢、

    Sathish。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    * 平台上有多路复用器、在 TX 路径上有 CAP、然后连接到 PCIe 连接器。

    谢谢、

    Sathish  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    根据数据表、该重定时器需要在外部为高速输入和输出实现交流耦合电容器。  中的交流耦合电容器
    100至220nF 的范围是足够的。

    谢谢、

    Rodrigo Natal

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好罗德里戈·纳塔尔、

    感谢您的支持。

    谢谢  

    Sathish。