This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TVS2200:我可以使用2个 TVS2200串联来形成高达44V 电平的浪涌保护器件吗?

Guru**** 2782645 points

Other Parts Discussed in Thread: TVS3300, TVS2200

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1064177/tvs2200-can-i-use-2-tvs2200-in-series-to-form-a-up-to-44v-level-surge-protection-device

器件型号:TVS2200
主题中讨论的其他器件:TVS3300

目前提供的平缓钳位器件的最大额定电压为33V (TVS3300)。  我可以使用2个 TVS2200串联构成高达44V 电平的浪涌保护器件吗?