This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN65DSI83:SN65DSI83稳定时序值

Guru**** 2756805 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1033744/sn65dsi83-sn65dsi83-stable-timing-value

器件型号:SN65DSI83

大家好、

对于 Innolux G156BGE-L03 15英寸 LCD 面板、
尝试调整 LVDS 时序的组合、但它不稳定、
当前的情况是、如果机器打开和关闭10次、LCD 屏幕或颜色平均将异常3~4次。
以下是调整后的时序、您能帮助查看并提供以下6组更好的时序建议值。
HSYNC 前沿= 82、HSYNC 后沿= 52、HSYNC 脉宽= 60
Vsync 前沿= 14、Vsync 后沿= 12、Hsync 脉冲宽度= 12
以上6组时序根据以下频率条件进行设置。
时钟频率= 76MHz、H_Active = 1366、V_Active = 768
HSYNC 极性= VSYNC 极性=正极性

Innolux G156BGE-L03的显示时序规格如下