请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DS34LV86T 大家好、
我们的客户希望了解 DS34LV86T 的以下两个方面:
1.它是否可与5V 信号(差分5V (RS-422)配合使用。
如果它与5V 信号一起使用、并且使用了失效防护电阻器、它们是被拉至+5V 和0v、还是+3.3V 和0v?
谢谢、
Jonathan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.