This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS250DF410:用于设计的 ds250df410基本评论。

Guru**** 2943430 points

Other Parts Discussed in Thread: DS250DF410

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/993300/ds250df410-ds250df410-basic-reveiw-for-design

器件型号:DS250DF410

大家好、  

我正在开发摄像头传感器硬件。

显影摄像头传感器是太高分辨率传感器(24MP)、无法与串行器/解串器一起传输。  

因此我对 mipi- csi2协议中的长传输数据感兴趣。

DS250DF410是否可以传输 mipi CSI-2质子?  

我的摄像头器件规格如下所示。

mipi- csi2  v1.2   

D-phy 4通道

数据速率  为2043Mbps/通道。  

分辨率: 5760 x 4312像素  

您能否建议如何在6米的距离内传输 mipi csi2协议?

谢谢、