This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TS3USBA225:来自 U7 PIN8和引脚10的 TS3USBA225RUTR 加上20-20kHz、100mV 扫描信号、引脚6和引脚12具有极高的失真度、高达30%。

Guru**** 2535750 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/763300/ts3usba225-ts3usba225rutr-from-u7-pin8-and-pin10-plus-20-20khz-100mv-sweep-signal-pin6-and-pin12-have-very-high-distortion-up-to-30

器件型号:TS3USBA225

插入 Line in 时、图1接地。            
Q2 S 和 D 极是导电的。            
芯片 U7引脚3 VCC 连接电池电压3.7V。       

同时、引脚11 SEL1也通过电阻 R16升高。            

VBUS 被挂起、因此 U7引脚7 SEL2为低电平。 U7切换到音频模式。
根据 U7 PIN8和引脚10 + 20-20kHz、100mV 扫描信号、引脚6和引脚12具有高达30%的极高失真度。