This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] HD3SS3415:温度

Guru**** 2810285 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/853566/hd3ss3415-temperature

器件型号:HD3SS3415

您好!

根据修订历史记录部分、将温度从:工业温度范围为–40°C 至85°C 更改为:工业温度范围为0°C 至70°C

此更改是否仅与性能相关,或者这是否是最大运行额定值?

例如,在-10°C 时为组件供电是否有问题(无需性能)?

此致、

Christian