Other Parts Discussed in Thread: DP83869HM
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DP83869HM 如果使用采用3电源配置的1G RGMII 铜质 DP83869HM。 以下是电压、
VDDIO = 1.8V
VDDA1P8 = 1.8V
VDDA2P5 =2.5V
VDD1P1 = 1.1V
然后、请针对每个电压建议典型电流消耗。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.