This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [FAQ] DP83822IF:光纤链路状态

Guru**** 2926990 points

Other Parts Discussed in Thread: DP83822HF, DP83822IF

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1272949/faq-dp83822if-fiber-link-status

器件型号:DP83822IF
主题中讨论的其他器件:DP83822HF

DP83822IF 和 DP83822HF 是 DP83822具有光纤功能的型号。

寄存器0x0001中的位2指示铜缆和光纤运行模式的链路状态。

在铜模式下、该寄存器按预期运行:位12将根据链路状态在"1"和"0"之间切换。

但是在光纤中、 当链路状态发生变化时、此位不会切换。 为了准确地检查链路状态、必须在读取寄存器0x0001之前执行软复位(设置寄存器0x001F = 4000)。