This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [常见问题解答] DP83TC812S-Q1:如何调整 MAC IO 的压摆率

Guru**** 2893300 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1309878/faq-dp83tc812s-q1-how-to-to-adjust-slew-rate-of-mac-ios

器件型号:DP83TC812S-Q1

降低 MAC 接口 IO 的压摆率可以改善某些频率的 EMC 发射。 这可以使用寄存器0x456来完成。

0x456位[5]和[0]分别控制 RX 和 TX MAC 接口焊盘的阻抗,这会影响压摆率。 0是快速模式、1是慢速模式。 这是唯一的两个选项、且位[9:6]和[4:1]无效。