Thread 中讨论的其他器件:UNIFLASH、CC3200、、 CC3100
你(们)好!
我 在 E2E 上只看到过几次此问题、没有实际的解决方案。
在尝试使用 UniFlash (3.1.1)连接至 CC3200时、获得以下信息:
[17:25:14] Begin ServicePackProgramming operation.[17:25:15] INFO: > Executing Operation: Connect[17:25:15] FATAL: --- Can't connect to device !! ---[17:25:18] FATAL: Error connecting to the device. Please check your COM port settings. Error code: 1[17:25:18] INFO: > Executing Operation: Disconnect[17:25:18] Operation ServicePackProgramming returned.[17:25:51] Begin ServicePackProgramming operation.[17:25:52] INFO: > Executing Operation: Connect[17:25:54] INFO: setting break signal[17:25:55] INFO: detecting FTDI for device reset[17:26:11] ERROR: ---reading ACK signal failed---...[17:52:46] WARNING: ---seting break signal to false failed---[17:52:48] INFO: setting break signal[17:52:49] INFO: detecting FTDI for device reset[17:53:05] ERROR: ---reading ACK signal failed---[17:53:05] WARNING: ---seting break signal to false failed---[17:53:05] FATAL: --- Can't connect to device !! ---[18:06:06] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3[18:06:06] INFO: > Executing Operation: Disconnect[18:06:06] Operation ServicePackProgramming returned.
我已经尝试了使用和不使用 SOP2跳线以及使用和不使用 J8-J11对 LaunchPad 进行复位。
我过去也成功地连接到了 MacOS 上的器件、但现在也出现了失败的 ACK、因为 CCS 调试器不再连接。 我也尝试了使用 cc3200tool 、但 ACK 也失败了。
有人能描述一下发生了什么事吗? 我怀疑 Launchpad 上的 FTDI 器件出了问题、但在文档中找不到足够的信息来了解它。
谢谢!