This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PCA9306:PCA9306DCUR

Guru**** 2931100 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1383550/pca9306-pca9306dcur

器件型号:PCA9306

工具与软件:

使用  PCA9306DCUR t0瞬态3.3V 至1.5V

如果主机(3.3V) 3mA 和从器件(1.5V) 3mA。

如何校准 Rpull(min)为1.5v?