This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN65DSI85:我们使用的是带有 imx93 (NXP) BSP 和 Linux 内核6.6.3版本的 SN65DSI85、是否有适用于 SN65DSI85的内核驱动程序?

Guru**** 2539500 points
Other Parts Discussed in Thread: SN65DSI85

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1383196/sn65dsi85-we-are-using-sn65dsi85-with-imx93-nxp-bsp-and-linux-kernel-version-6-6-3-is-there-any-kernel-driver-available-for-sn65dsi85

器件型号:SN65DSI85

工具与软件:

您好、团队:

我们将 SN65DSI85与 imx93 ( NXP ) Linux 内核版本6.6.3一起使用是否有适用于 SN65DSI85的内核驱动程序?

请建议如何将 SN65DSI85与 imx93 ( NXP ) Linux 内核版本6.6.3一起使用。

www.nxp.com/.../embedded-linux-for-i-mx-applications-processors:IMXLINUX

谢谢

Gopal