This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DS90UB929-Q1EVM:DS90UB948-Q1EVM 的显示器保持黑色

Guru**** 2874030 points

Other Parts Discussed in Thread: DS90UB948-Q1EVM, DS90UB949-Q1EVM, ALP, DS90UB929-Q1EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1431132/ds90ub929-q1evm-display-with-ds90ub948-q1evm-remains-black

器件型号:DS90UB929-Q1EVM
主题中讨论的其他器件:DS90UB948-Q1EVMDS90UB949-Q1EVMALP、

工具与软件:

带有解串器的显示器:DS90UB948-Q1EVM
串行器:DS90UB949-Q1EVM

ALP +配置文件更新:v1.57.0010

串行器设置为默认配置:

串行器寄存器:

[REGISTERS]
Device = ALP Nano 1 - DS90UB949, Connector 1
Comments = "DS90UB949-Q1EVM_TDS"
Date = 10/25/2024
Time = 15:28:58
Reg = 0,0x0000,0x18
Reg = 0,0x0001,0x00
Reg = 0,0x0003,0xDA
Reg = 0,0x0004,0x80
Reg = 0,0x0005,0x00
Reg = 0,0x0006,0x58
Reg = 0,0x0007,0xA0
Reg = 0,0x0008,0xB0
Reg = 0,0x0009,0x00
Reg = 0,0x000A,0x13
Reg = 0,0x000B,0x00
Reg = 0,0x000C,0x07
Reg = 0,0x000D,0x20
Reg = 0,0x000E,0x00
Reg = 0,0x000F,0x00
Reg = 0,0x0010,0x00
Reg = 0,0x0011,0x00
Reg = 0,0x0012,0x00
Reg = 0,0x0013,0x99
Reg = 0,0x0014,0x00
Reg = 0,0x0015,0x01
Reg = 0,0x0016,0xFE
Reg = 0,0x0017,0x1E
Reg = 0,0x0018,0x7F
Reg = 0,0x0019,0x7F
Reg = 0,0x001A,0x09
Reg = 0,0x001B,0x00
Reg = 0,0x001C,0x00
Reg = 0,0x001D,0x00
Reg = 0,0x001E,0x05
Reg = 0,0x001F,0xF7
Reg = 0,0x0020,0x0B
Reg = 0,0x0021,0x00
Reg = 0,0x0022,0x25
Reg = 0,0x0023,0x00
Reg = 0,0x0024,0x00
Reg = 0,0x0025,0x00
Reg = 0,0x0026,0x00
Reg = 0,0x0027,0x00
Reg = 0,0x0028,0x01
Reg = 0,0x0029,0x20
Reg = 0,0x002A,0x20
Reg = 0,0x002B,0xA0
Reg = 0,0x002C,0x00
Reg = 0,0x0030,0x00
Reg = 0,0x0031,0x00
Reg = 0,0x0032,0x00
Reg = 0,0x0033,0x00
Reg = 0,0x0034,0x00
Reg = 0,0x0035,0x00
Reg = 0,0x0036,0x00
Reg = 0,0x0037,0x00
Reg = 0,0x0038,0x00
Reg = 0,0x0039,0x00
Reg = 0,0x003A,0x00
Reg = 0,0x003B,0x00
Reg = 0,0x003C,0x00
Reg = 0,0x003D,0x00
Reg = 0,0x003E,0x00
Reg = 0,0x003F,0x00
Reg = 0,0x0040,0x14
Reg = 0,0x0041,0x5C
Reg = 0,0x0042,0x00
Reg = 0,0x0043,0x00
Reg = 0,0x0044,0x80
Reg = 0,0x0045,0x00
Reg = 0,0x0046,0x00
Reg = 0,0x0047,0x00
Reg = 0,0x0048,0x01
Reg = 0,0x0049,0x68
Reg = 0,0x004A,0x01
Reg = 0,0x004B,0x38
Reg = 0,0x004C,0x04
Reg = 0,0x004D,0x00
Reg = 0,0x004E,0x00
Reg = 0,0x004F,0x00
Reg = 0,0x0050,0x97
Reg = 0,0x0051,0xA1
Reg = 0,0x0052,0x1E
Reg = 0,0x0053,0x00
Reg = 0,0x0054,0x09
Reg = 0,0x0055,0x0C
Reg = 0,0x0056,0x15
Reg = 0,0x0057,0x00
Reg = 0,0x0058,0x00
Reg = 0,0x0059,0x00
Reg = 0,0x005A,0xCD
Reg = 0,0x005B,0x60
Reg = 0,0x005C,0x02
Reg = 0,0x005D,0x06
Reg = 0,0x005E,0x44
Reg = 0,0x005F,0x96
Reg = 0,0x0060,0x22
Reg = 0,0x0061,0x02
Reg = 0,0x0062,0x00
Reg = 0,0x0064,0x10
Reg = 0,0x0065,0x00
Reg = 0,0x0066,0x00
Reg = 0,0x0067,0x00
Reg = 0,0x0068,0x00
Reg = 0,0x0069,0x00
Reg = 0,0x006A,0x00
Reg = 0,0x006B,0x00
Reg = 0,0x006C,0x00
Reg = 0,0x0070,0x00
Reg = 0,0x0071,0x00
Reg = 0,0x0072,0x00
Reg = 0,0x0073,0x00
Reg = 0,0x0074,0x00
Reg = 0,0x0075,0x00
Reg = 0,0x0076,0x00
Reg = 0,0x0077,0x00
Reg = 0,0x0078,0x00
Reg = 0,0x0079,0x00
Reg = 0,0x007A,0x00
Reg = 0,0x007B,0x00
Reg = 0,0x007C,0x00
Reg = 0,0x007D,0x00
Reg = 0,0x0080,0x00
Reg = 0,0x0081,0x00
Reg = 0,0x0082,0x00
Reg = 0,0x0083,0x00
Reg = 0,0x0084,0x00
Reg = 0,0x0090,0x00
Reg = 0,0x0091,0x00
Reg = 0,0x0092,0x00
Reg = 0,0x0093,0x00
Reg = 0,0x0094,0x00
Reg = 0,0x0098,0x00
Reg = 0,0x0099,0x00
Reg = 0,0x009A,0x00
Reg = 0,0x009B,0x00
Reg = 0,0x009C,0x00
Reg = 0,0x009D,0x00
Reg = 0,0x009E,0x00
Reg = 0,0x009F,0x00
Reg = 0,0x00A0,0x00
Reg = 0,0x00A1,0x00
Reg = 0,0x00A2,0x00
Reg = 0,0x00A3,0x00
Reg = 0,0x00C0,0x00
Reg = 0,0x00C1,0x00
Reg = 0,0x00C2,0xA8
Reg = 0,0x00C3,0x00
Reg = 0,0x00C4,0x68
Reg = 0,0x00C5,0x00
Reg = 0,0x00C6,0x00
Reg = 0,0x00C7,0xE0
Reg = 0,0x00C8,0xC0
Reg = 0,0x00C9,0x00
Reg = 0,0x00CA,0x00
Reg = 0,0x00CB,0x00
Reg = 0,0x00CC,0x00
Reg = 0,0x00CE,0xFF
Reg = 0,0x00D0,0x00
Reg = 0,0x00D1,0xA1
Reg = 0,0x00D2,0x00
Reg = 0,0x00D3,0x46
Reg = 0,0x00E0,0x00
Reg = 0,0x00E1,0x00
Reg = 0,0x00E2,0xA8
Reg = 0,0x00E3,0x00
Reg = 0,0x00E4,0x68
Reg = 0,0x00E5,0x38
Reg = 0,0x00E6,0x00
Reg = 0,0x00E7,0x20
Reg = 0,0x00F0,0x5F
Reg = 0,0x00F1,0x55
Reg = 0,0x00F2,0x42
Reg = 0,0x00F3,0x39
Reg = 0,0x00F4,0x34
Reg = 0,0x00F5,0x39
Reg = 0,0x00F6,0x00
Reg = 0,0x00F8,0x00
Reg = 0,0x00F9,0x00

解串器的寄存器(显示):

[REGISTERS]
Device = ALP Nano 1 - DS90UB948, Connector 1
Comments = "DS90UB948_Q1EVM_1920*1080"
Date = 10/25/2024
Time = 15:32:56
Reg = 0,0x0000,0x58
Reg = 0,0x0001,0x04
Reg = 0,0x0002,0x00
Reg = 0,0x0003,0xF0
Reg = 0,0x0004,0xFE
Reg = 0,0x0005,0x1E
Reg = 0,0x0006,0x00
Reg = 0,0x0007,0x18
Reg = 0,0x0008,0x00
Reg = 0,0x0009,0x00
Reg = 0,0x000A,0x00
Reg = 0,0x000B,0x00
Reg = 0,0x000C,0x00
Reg = 0,0x000D,0x00
Reg = 0,0x000E,0x00
Reg = 0,0x000F,0x00
Reg = 0,0x0010,0x00
Reg = 0,0x0011,0x00
Reg = 0,0x0012,0x00
Reg = 0,0x0013,0x00
Reg = 0,0x0014,0x00
Reg = 0,0x0015,0x00
Reg = 0,0x0016,0x00
Reg = 0,0x0017,0x00
Reg = 0,0x0018,0x00
Reg = 0,0x0019,0x01
Reg = 0,0x001A,0x00
Reg = 0,0x001B,0xF5
Reg = 0,0x001C,0x3B
Reg = 0,0x001D,0x10
Reg = 0,0x001E,0x00
Reg = 0,0x001F,0x00
Reg = 0,0x0020,0x00
Reg = 0,0x0021,0x00
Reg = 0,0x0022,0x40
Reg = 0,0x0023,0x20
Reg = 0,0x0024,0x08
Reg = 0,0x0025,0x00
Reg = 0,0x0026,0x14
Reg = 0,0x0027,0x26
Reg = 0,0x0028,0x19
Reg = 0,0x0029,0x00
Reg = 0,0x002A,0x00
Reg = 0,0x002B,0x00
Reg = 0,0x002C,0x00
Reg = 0,0x002D,0x00
Reg = 0,0x002E,0x00
Reg = 0,0x002F,0x00
Reg = 0,0x0030,0x00
Reg = 0,0x0031,0x00
Reg = 0,0x0032,0x90
Reg = 0,0x0033,0x25
Reg = 0,0x0034,0x01
Reg = 0,0x0035,0x00
Reg = 0,0x0036,0x00
Reg = 0,0x0037,0x8D
Reg = 0,0x0038,0x00
Reg = 0,0x0039,0x00
Reg = 0,0x003A,0x00
Reg = 0,0x003B,0x00
Reg = 0,0x003C,0x20
Reg = 0,0x003D,0xE0
Reg = 0,0x003E,0x23
Reg = 0,0x003F,0x00
Reg = 0,0x0040,0x43
Reg = 0,0x0041,0x03
Reg = 0,0x0042,0x03
Reg = 0,0x0043,0x00
Reg = 0,0x0044,0x60
Reg = 0,0x0045,0x88
Reg = 0,0x0046,0x00
Reg = 0,0x0047,0x00
Reg = 0,0x0048,0x0F
Reg = 0,0x0049,0x81
Reg = 0,0x004A,0x00
Reg = 0,0x004B,0x08
Reg = 0,0x004C,0x00
Reg = 0,0x004D,0x00
Reg = 0,0x004E,0x63
Reg = 0,0x004F,0x00
Reg = 0,0x0050,0x03
Reg = 0,0x0051,0x10
Reg = 0,0x0052,0x00
Reg = 0,0x0053,0x01
Reg = 0,0x0054,0x80
Reg = 0,0x0055,0x00
Reg = 0,0x0056,0x00
Reg = 0,0x0057,0x00
Reg = 0,0x0058,0x00
Reg = 0,0x0059,0x7F
Reg = 0,0x005A,0x20
Reg = 0,0x005B,0x20
Reg = 0,0x005C,0x00
Reg = 0,0x005D,0x00
Reg = 0,0x005E,0x00
Reg = 0,0x005F,0x00
Reg = 0,0x0060,0x00
Reg = 0,0x0061,0x00
Reg = 0,0x0062,0x00
Reg = 0,0x0063,0x00
Reg = 0,0x0064,0x10
Reg = 0,0x0065,0x00
Reg = 0,0x0066,0x00
Reg = 0,0x0067,0x00
Reg = 0,0x0068,0x00
Reg = 0,0x0069,0x00
Reg = 0,0x006E,0x00
Reg = 0,0x006F,0x00
Reg = 0,0x0070,0x00
Reg = 0,0x0071,0x00
Reg = 0,0x0072,0x00
Reg = 0,0x0073,0x07
Reg = 0,0x0074,0x07
Reg = 0,0x0075,0x08
Reg = 0,0x0076,0x00
Reg = 0,0x0077,0x00
Reg = 0,0x0078,0x00
Reg = 0,0x0079,0x00
Reg = 0,0x007A,0x00
Reg = 0,0x007B,0x6D
Reg = 0,0x007C,0x02
Reg = 0,0x0080,0x00
Reg = 0,0x0081,0x00
Reg = 0,0x0082,0x00
Reg = 0,0x0083,0x00
Reg = 0,0x0084,0x00
Reg = 0,0x0090,0x00
Reg = 0,0x0091,0x00
Reg = 0,0x0092,0x00
Reg = 0,0x0093,0x00
Reg = 0,0x0094,0x00
Reg = 0,0x0098,0x00
Reg = 0,0x0099,0x00
Reg = 0,0x009A,0x00
Reg = 0,0x009B,0x00
Reg = 0,0x009C,0x00
Reg = 0,0x009D,0x00
Reg = 0,0x009E,0x00
Reg = 0,0x009F,0x00
Reg = 0,0x00C0,0x00
Reg = 0,0x00C1,0x00
Reg = 0,0x00C3,0x00
Reg = 0,0x00C4,0x00
Reg = 0,0x00C5,0x00
Reg = 0,0x00C8,0xC0
Reg = 0,0x00C9,0x00
Reg = 0,0x00CA,0x00
Reg = 0,0x00CB,0x00
Reg = 0,0x00CC,0x00
Reg = 0,0x00E0,0x00
Reg = 0,0x00E1,0x00
Reg = 0,0x00E2,0x00
Reg = 0,0x00E3,0x00
Reg = 0,0x00E8,0x00
Reg = 0,0x00E9,0x00
Reg = 0,0x00EA,0x00
Reg = 0,0x00F0,0x5F
Reg = 0,0x00F1,0x55
Reg = 0,0x00F2,0x42
Reg = 0,0x00F3,0x39
Reg = 0,0x00F4,0x34
Reg = 0,0x00F5,0x38
Reg = 0,0x00F6,0x00
Reg = 0,0x00F8,0x00
Reg = 0,0x00F9,0x00

ALP 软件:

 我已断开 HDMI 源并尝试使用"图形发生器"。 但是、只有在中、才会打开"Pattern Generator"选项卡 ALP 配置文件更新 正弦值 不会 已安装。

即使显示了该选项卡、串行器 DS90UB929-Q1EVM 是否没有"Pattern Generator"(图形发生器)?

或者、是否有其他方法可以获取正确的配置以使我的显示器正常工作?

因为我已经尝试了很多我在论坛上找到的东西,到目前为止没有任何工作。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Iris、

    [报价 userid="627440" url="~/support/interface-group/interface/f/interface-forum/1431132/ds90ub929-q1evm-display-with-ds90ub948-q1evm-remains-black "] 我已断开 HDMI 源并尝试使用"图形发生器"[/报价]

    您可以在打开"Patgen Registers"选项卡之前重试吗?

    我认为、在能够配置 Patgen GUI 之前、必须先对寄存器进行实例化。

    请告诉我您找到的结果。

    此致!

    Miguel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Miguel:

    非常感谢。

    这解决了我的问题与"图形生成器"选项卡:-)

    现在、我可以看看我的黑色显示器问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我尝试了用于"HD 1080p 60Hz"的可用配置的图形发生器、但在显示器上未发生任何事情。

    我检查了在未插入 HDMI 电缆时是否有其他问题。
    我注意到在"HDMI"选项卡中、"FDPP3"状态仅显示"Single Port0"、而不显示"Dual FPD3"。

    但是、如果我正确读取解串器的寄存器、则需要"双 FDP3":



    这是否正常? 或者与解串器的连接是否未正确建立?
    我还尝试通过"强制双路"更改"链路模式"。 很遗憾、这不起作用。 "链接模式"没有改变。


    顺便说一下、我注意到"桥接控制设置"区域中的"FDP 音频模式"和"FDP-Link III 模式"的名称可能混在一起:

    另一个问题:为了通过"图形发生器"在串行器和解串器之间进行通信、是否必须在串行器上设置 EDID?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Iris、

    在您的 PATGEN from SER 过程中、我会检查以下两项:

    1) 1) SER 和 DES 器件之间是否存在锁定?

    您可以在 ALP 中查看这一点、我建议:

    1. 在948器件上、读取常规状态0x1C 应返回 DUAL_RX_STS 高电平、发送 PATGEN 后 LOCK 也应为高电平。
      1. 此时、Info 选项卡还应该会显示948作为合作伙伴器件。
      2. 如果发送器双链路状态为高电平、则我认为这表示可以启用菊花链、如果这是唯一的 DES、则应禁用菊花链。
    2. 在949器件上、您可以读取0x0c 以了解器件的链路状态、只是确认器件已使用 DES 锁定。
    3. 检查双模硬件是否正确配置 SER 和 DES 之间的 FPD-Link、并检查 DES 菊花链是否禁用。

    2)显示规格是否与 PATGEN 编程相匹配?

    仔细检查分辨率、消隐周期和 PCLK 都处于输出的限制范围内。 某些显示可能需要严格的消隐参数。

    在外部时钟/时序不可用作输入的情况下、您可能还希望将内部模式与内部时钟结合使用。

    不必设置 EDID、因为 PATGEN 发生器使用内部 BIST 从 SER 发送数据。

    请随时向我通报最新结果!

    此致!

    Miguel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Miquel:

    1) SER 和 DES 器件之间是否锁定?

    是的、发送 PATGEN 时、DUAL_RX_STS 和 LOCK 为高电平、两侧都正确识别双链路状态。
    但显示屏仍然显示为黑色。

    2)显示规格是否与 PATGEN 编程匹配?

    是的、我直接从 EDID 中提取了显示规格。 "HD 1080p 60Hz"的默认设置也适用于我的显示屏。

    只有在我设置 EDID、连接 HDMI 并重新启动图形发生器后、我才能够在显示屏上看到测试图形的颜色。

    完成图形发生器设计后、我还可以在显示屏上看到笔记本电脑屏幕。

    您似乎必须按特定顺序打开和配置设备、才能在显示屏上显示图像:

    1. 打开解串器+串行器
    2. 将 EDID 信息写入串行器
    3. 插入 HDMI 源
    4. 在 ALP 软件中:
      1. 开模式寄存器
      2. 打开图形发生器并正确配置
      3. 然后启动生成器(测试图像可见)并再次停止生成器

    或:

    1. 打开串行器
    2. 将 EDID 信息写入串行器
    3. 插入 HDMI 源
    4. 打开解串器。

    我很高兴现在可以在显示屏上看到的不仅仅是黑屏。

    但如果没有 HDMI 源、我仍然看不到测试图片、或者至少打开背光。
    这是否正常? 或者我还缺少什么吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Iris、

    图形发生器时序可能已设置为外部时钟源?

    在外部时钟模式下、图形发生器将配置为内部时序参数(分辨率)、同时接收并使用外部时钟信号。 内部时序模式将产生控制寄存器中配置的时钟。  

    查看您是否可以将这些设置用于图形发生器、以确定您是否仍需要 HDMI 源才能在 DES -显示屏上产生输出。

    此致!

    Miguel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Miguel:

    我已经尝试过更改时钟信号源、但它没有改变任何内容。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Iris、

    我看到的、看起来内部 PCLK 发生器可能超出了显示器需求的技术规格范围。

    如果您尝试了上述配置、且内部时序规格为1080p (60Hz)的系统无法正常工作、那么我会说显示器可能需要 HDMI 提供的特定时序。

    您能仔细检查一下显示屏规格吗?

    如果使用内部时序、使用 M 因子3和 N 因子4应该产生150 MHz 的 PCLK、该 PCLK 将用于驱动需要具有预编程1080p 时序的148.5 MHz PLCK 的近似时序。

    请告诉我您对此的想法。

    此致!

    Miguel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Miguel:

    根据"Information"选项卡、当连接 HDMI 视频源时、PCLK 为大约150MHz。 因此、我尝试了该值。
    但不幸的是、没有任何变化。

    我还尝试了其他 PCLK 频率、但只要显示器是黑色、就无法正常工作。

    只要我连接了 HDMI 源、显示屏上的背景就会亮起。 我还能够将图形发生器与"Timing Source:internal"配合使用。
    即使没有连接 HDMI 源也是如此。

    我想在没有 HDMI 源的情况下打开显示屏时会遇到问题。

    是否有解决此问题的已知解决方案?

    此致!
    Iris

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Iris、

    我将了解为什么除非涉及到源、否则图形不会显示。 请给我1-2个工作日进行调查。

    此致!

    Miguel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Iris、

    您是否能够分享显示屏所使用的时序规格? 我怀疑针对这个时间的 PCLK 要求也许是严格的、这就是为什么使用 HDMI 源也许适合于此应用、但是当在模式生成期间手工生成它时、对接会遇到问题。

    此致!

    Miguel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Miguel:

    很抱歉、我们花了很长时间才回复您。 我不得不请求允许分享时序规格。

    我只能分享显示器制造商提供给我的 EDID 以及我个人通过 AW EDID 编辑器生成的 EDID。

    很遗憾、制造商提供的 EDID 包含另一个显示器。 这就是它不能用于单个1920x1080显示器的原因。

    0x00, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0x00, 0x31, 0xD8, 0x00, 0x00, 0x01, 0x00, 0x00, 0x00,
     0x17, 0x10, 0x01, 0x04, 0xA5, 0x1C, 0x0C, 0x78, 0xE6, 0xCB, 0x05, 0xA4, 0x55, 0x4C, 0x9A, 0x27,
     0x10, 0x50, 0x54, 0x00, 0x00, 0x00, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01,
     0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x72, 0x41, 0x60, 0x96, 0x90, 0x38, 0x0F, 0x40, 0x32, 0x32,
     0x55, 0x00, 0xDC, 0x78, 0x00, 0x00, 0x00, 0x18, 0x00, 0x00, 0x00, 0xFD, 0x00, 0x3B, 0x3D, 0x40,
     0x42, 0x30, 0x01, 0x0A, 0x20, 0x20, 0x20, 0x20, 0x20, 0x20, 0x00, 0x00, 0x00, 0xFC, 0x00, 0x42,
     0x4A, 0x45, 0x56, 0x20, 0x64, 0x69, 0x73, 0x70, 0x6C, 0x61, 0x79, 0x0A, 0x00, 0x00, 0x00, 0xF7,
     0x00, 0x0A, 0x00, 0x00, 0x00, 0x00, 0x01, 0x0A, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xE5


    然后、我根据提供的 EDID 为1920x1080显示器创建了我自己的 EDID。 当使用 Windows 笔记本电脑作为 HDMI 源时、此方法有效。

    0x00, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0x00, 0x34, 0x27, 0x01, 0x00, 0x01, 0x00, 0x00, 0x00,
     0x28, 0x22, 0x01, 0x04, 0xA2, 0x16, 0x0C, 0x78, 0xE7, 0xEE, 0x95, 0xA3, 0x54, 0x4C, 0x99, 0x26,
     0x0F, 0x50, 0x54, 0x00, 0x00, 0x00, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01,
     0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x29, 0x36, 0x80, 0xA0, 0x70, 0x38, 0x1F, 0x40, 0x30, 0x20,
     0x35, 0x00, 0xDF, 0x7D, 0x00, 0x00, 0x00, 0x18, 0x00, 0x00, 0x00, 0xFD, 0x00, 0x17, 0xF0, 0x0F,
     0xFF, 0x0E, 0x00, 0x0A, 0x20, 0x20, 0x20, 0x20, 0x20, 0x20, 0x00, 0x00, 0x00, 0xFC, 0x00, 0x54,
     0x44, 0x53, 0x5F, 0x31, 0x39, 0x32, 0x30, 0x78, 0x31, 0x30, 0x38, 0x30, 0x00, 0x00, 0x00, 0x10,
     0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x23

    我希望这些信息会有所帮助。

    此致!
    Iris

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Iris、

    让我复查此 EDID 时序、以确定是否可通过949的内部 CLK PATGEN 实现 PCLK。

    此致!

    Miguel