This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO6520:输入引脚钳位二极管电流额定值

Guru**** 2974170 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1573497/iso6520-input-pin-clamp-diode-current-ratings

器件型号:ISO6520


工具/软件:

如果 INx 超过 Vccx+0.5、是否可以依赖这些结构来控制受 PW 电阻器(例如 1mA 至<xmt-block1> 5mA</xmt-block>) 限制 5mA 限制的)的少量连续电流?