This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO6740-Q1:ISO6740FQDWRQ1 - VCC1 工作电压的四元导通。

Guru**** 2964790 points

Other Parts Discussed in Thread: ISO6740-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1574342/iso6740-q1-iso6740fqdwrq1---quary-on-vcc1-operating-voltage

器件型号:ISO6740-Q1


工具/软件:

您好的团队、

由于存在两组工作电压、ISO6740-Q1 能否与 VCC1 侧 (1.8V) 和 VCC2 侧 (5V) 一起使用

谢谢、

pream