This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO1212:AC/DC 电压检测

Guru**** 2928980 points

Other Parts Discussed in Thread: ISO1212

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1638514/iso1212-ac-dc-voltage-sense

器件型号: ISO1212

您好、  

我有设计要求来检测“通用“输入、而不管 24VDC 或 240VAC(这意味着输入可以是 24VDC 或 240VAC,直到连接的负载)。 此 ISO1212 或任何其他 IC 是否适合此应用?