This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO7821:VCC1和VCC2的电源不同

Guru**** 2694555 points

Other Parts Discussed in Thread: ISO7821

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1103153/iso7821-different-power-supply-for-vcc1-and-vcc2

部件号:ISO7821

大家好,

我有一个关于VCC1和VCC2的问题。

当VCC1和VCC2使用不同的电源时,ISO7821是否正常工作?

(例如 VCC1=3.3V,VCC2=5V)

 

此致,

YUto