This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 模拟隔离放大器

Guru**** 2601915 points
Other Parts Discussed in Thread: AMC1351

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1115272/analog-isolation-amplifiers

主题中讨论的其他器件:AMC1351
正在寻找具有以下规格的模拟隔离放大器
模拟输入电压: 0至5V
模拟输出电压:0至5V
隔离: 最小1500Vrms
输入: 来自压力传感器和温度传感器
带宽:最大2kHz
精度:1%
非线性度:0.5%
经 UL 认证