This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO7760:电源

Guru**** 2831025 points

Other Parts Discussed in Thread: ISO7760

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1007965/iso7760-power-supply

器件型号:ISO7760

您好!

你好。

ISO7760的初级侧和次级侧以及类似数字隔离器(例如5V 初级侧和3V 次级侧)是否可以使用不同的电源?

谢谢你。

此致、

Cedrick