This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO7762:电源电压要求

Guru**** 2530250 points
Other Parts Discussed in Thread: ISO7762

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/999657/iso7762-supply-voltage-requirements

器件型号:ISO7762

您好!

我对 ISO7762有一些不确定的设计要求。

我想确保、如果输入电压为5V 时 VCC2的电源电压可以是3.3V、那么该模式下的电源电流特性是什么?

对于输出信号、它可以直接连接到 MCU、还是需要添加一个小型串行电阻器? 谢谢。

此致、

小燕