Other Parts Discussed in Thread: SN6501
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SN6505B 主题中讨论的其他器件:SN6501
大家好、
是否有办法将 SN6505的电流限制更改为较低的电流限制?
但不像 SN6501那么低。 客户需要大约0.9A 典型值和1.1A 最大值的电流限制
此致、
Jon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.