This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO6740:在特定的工业应用中需要光耦合器。

Guru**** 2782615 points

Other Parts Discussed in Thread: ISO6740

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1355732/iso6740-need-optocoupler-for-the-specific-industrial-appliczations

器件型号:ISO6740

大家好、晚上好、


您能为满足下列针对工业应用的要求提供建议、光耦合器器件型号吗?

隔离电压      >1000V
隔离电阻10M 欧姆@施加电压1000V
符合 IEC 60664-1的 II 污染等级
-根据 IEC 60664-1定义的过电压类别 II
-工作温度20至60°C

此致、

桑盖塔